We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I have a small 5 v DC device I’m trying to power. Because my Elite Notebook is too old to work with Microchip PIC4, I’m trying to use a blinking LED to control the powering of the devise. The idea is for the blinking LED to turn the the device with 1, 5 v DC motor to turn on and off.,
My plan was to have power pass through to On/Off blinking LED. Then tried with and without power a Capacitor to increase the voltage and milliamps to power the activation side of the TLP222AF-ND. It is a SSR Relay.
Then on the load side, I wanted to control powering on and off for a 5v vibrator motor. However, when trying to use it like this I cannot get any blinking on the load end. I only get nothing or constantly on.
I need help to get the device blinking without using a microcontroller due to my limitation on the Elite Notebook
Hi Doug, Welcome back to Digi-Key TechForum. My apologies for this delayed response. We are reviewing your request. Are you able to provide us with a photo of your circuit to help us understand where the LED is located in the circuit and where it is located in reference with the output? What are the specifications of the LED? Thank you Mo
I will check them out. If they are small, that may work. Here are 3 types of components that may work for my on/off without a microcontroller… I’m not really sure because I don’t design circuits. I have a project coming out that has a budget. I will have a very complexe microcontroller program.
Let me know if you may be interested in helping.
Using a 555 timer will work to control the frequency switching of your SSR. The datasheet of the 555 timer you choose should explain how to use it, and create the frequency you want.
As a side note, self-blinking LEDs voltage will remain constant and not change, therefore it cannot be used to control external circuitry. it is only the current that will fluctuate leading up to the LED. It will usually fluctuate from micro amps (LED off) to milli amps (LED ON).
The flashing LED uses an internal circuit to flash so will not work to turn a circuit on and off. Using a capacitor on the input side will hold the input circuit on until it discharges below the threshold which may not be desirable.
Use a 555 timer and a current limiting resistor to drive the input diode inside the SSR. There are many examples of 555 LED flashers on the net and Digi-Key has all of the components you need. The beauty of the 555 is that it is adjustable so you can tune in your flash rate.