Part number : LED40W-045-C0900-D

Hi Sir,

Please help us to check this part no: LED40W-045-C0900-D , did it come with LED? if not , please kindly provide us the part number with LED.

Thank you.

Part number LED40W-045-C0900-D is an LED driver. No LED is included.

Selection of an appropriate LED or array of such for use with this device is a task left to the user, because the number of possible options, combinations, and configurations is nearly infinite.

Dear Rick,

Thank you for your reply .

Can you help to provide us the part number which was include LED one .

Thank you very much .

Thank you and have a great day ahead.

Hi Rick,

Thank you for promptly reply, can you provide us the part number, which was your mention one (configurations) to combinations it or did you any part number which was 2 in 1 , so that we can going to telling End-user and let they decide it . Thank you .

There are no related part numbers for this driver that include an LED.

This product family contains LED items of the type most commonly used, but custom LED assemblies built from products in this family are also possible.