Photomicrosensors do not work. Please advise possible causes and countermeasures

Question:

After delivery, some Photomicrosensors do not work. Please advise possible causes and countermeasures.

Block

Answer:

One of the causes is estimated to be a decrease in light current due to aging of the Photomicrosensors LED. In this case, the circuit design should be reviewed.

Block

Explanation:

LED elements have the characteristic that the light emission output gradually decreases over time. Because the Photomicrosensors use a non-contact detection method, they have higher reliability than mechanical switches and are effective in extending the life of equipment. However, it is based on a circuit design that takes into account the aging of the LED. By setting a threshold with sufficient margin, stable detection over a long period of time can be performed on the equipment.
For details, refer to Thecnical Information for Photomicrosensors as well as the following related FAQ.

Block


Product category

Sensors Photomicro Sensors


Classification

Trouble shootings


Related keywords

Optical Sensor
Trouble Shooting
Products Which Can Not Detect
LED Degradation
Light-Emitting Power
Light Current
Life-Time Extension?
Stable Sensing

Block

Please visit the link below to see this product line on the Digi-Key website
Optical Sensors | Digi-Key Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/sensors/FAQE40028