What is the inlet and the outlet Diameter of the pipe.
Hello Bharat,
Welcome to community!
Please share Part number of the pipe.
4165-CS949-104-N-0A-ND
Pipe Dimensions are 24.00" L x 5.00" W x 0.38" H (609.6mm x 127.0mm x 9.7mm)
Kindly check link for drawing and dimension.
Ok thanks for the dimensions, I want to ask that can I use it for both the purpose like heating and cooling. If I can, then what equipment I have required to cool or heat this, if you have the equipment link, please provide me
Hello bharat.kachhawa,
The 4165-CS949-104-N-0A-ND can surely be used to heat or cool the Plate, but it was designed for cooling. What gets hooked to this is up to the customer. If you want some ideas, maybe one of the engineers can add to this post.
They will need to know exactly what you are working on, and what you want to accomplish.
Exactly I can’t tell but assume the water, which is already heated, I want to cool it so is their additional source (like Peltier cooler) required to cool the water, if yes, then What is it?
Can you provide me the num on which is can directly call you.
You can call us at 1-800-344-4539 and ask to speak to a tech. Or you can call the tech department directly by calling 1-218-681-6674 and extension 55009.