Please advise the appropriate amount of pushing for a basic switch

Question:

Please advise the appropriate amount of pushing for a basic switch.

Block

Answer:

If an operating body stops near the operating position (OP) or the releasing position (RP) of a basic switch, it may create chattering or bouncing and cause problems. Set the switch within the allowable operation speed (catalog value) so as not to stop at the OP point and RP point.

Block

Explanation:

The operating stroke is the movement of the actuator caused by the operating body that is required for the switch to operate correctly. Operate the unit smoothly as described below, and do not stop its movement near the operating position (OP) or releasing position (RP). Set the switch pushing distance from 60% to 90% of the specified overtravel (OT) value. Beyond 90%, the actuator or switch may be damaged.

  1. The actuator must normally be in the free position (FP). (The operating body is separated from the actuator.)
  2. The motion of the operating body must not stop at the operating position (OP) and the releasing position (RP).
  3. When the operation reverse position (suitable pushing of the actuator) is set, the motion of the operating body must be adjustable based on the specified overtravel (OT) value.
  4. When the switch is placed in a device, the suitable pushing point of the operating body has to be 60% to 90% in the operating position (OP) to the total travel position (TTP).

Block

Product category

Switches Basic Switches


Classification

Trouble shootings


Related keywords

Basic Switch
Operating Stroke
Operating Speed
Operating Position
Releasing Position
Allowable Operation Speed

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20046