What are basic switches with a long stroke?

Question:

What are basic switches with a long stroke?

Block

Answer:

The stroke of a basic switch is basically proportional to the size of the switch. Therefore, the longer (larger) the stroke of the basic switch you select, the larger the switch becomes. However, the lever actuator makes the stroke longer (larger) even if the switch is small. The longer the lever actuator is, the longer (larger) the stroke becomes while the smaller the OF (operating force) and RF (release force) become. As a result, when the OF is reduced, you need to select a lever actuator.

Block

Explanation:

The V-type and S-type switches are pushbutton types with almost the same stroke, and the lever actuator increases the stroke.
D2HW, D2QW, and D2AW have a longer stroke compared to the size of the switch, making it easier to set.
Please note that D2HW, D2QW, and D2AW models have achieved a small long stroke with their unique structure.

Full stroke of switch:

V size (common to pushbutton/lever): Stroke = PT+OT
S size/J size (pushbutton): Stroke = PT + OT
S size/J size (lever): Stroke = (FP-OP) + OT

Block

Quick tips

The larger the PT, the more allowance (margin of variation) is attained in the setting (operating point).
A small long-stroke model (D2HW, D2QW, D2AW) is recommended when the installation space is small.
Please note that they have no high-capacity switching. Please check the electrical load.

For more information, see Product pages.


Product category

Switches Basic Switches


Classification

Selection, Characteristics


Related keywords

Basic Switch
Small Long Stroke
Operating Force
Release Force

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20006