Dear sir,
please help me to find out following attached part marked images and send the full part numbers
- VJ-6pin
- CBAH-5 PIN
- EGAD HSB-6PIN
Hello @pottenenir,
Thank you for the images.
I am not able to exactly pinpoint the part with the CBA marking, but the most common item with that marking is a DC/DC converter in the SOT-25 package. It might be XC9235B1ACMR-G from Torex. XC9235B1ACMR-G Torex Semiconductor Ltd | Integrated Circuits (ICs) | DigiKey
I was not able to verify the other two part numbers.
Hi, pottenenir.
Check the VJ-6pin chip again.
Unsolder it and check the pins carefully.
There should be 5 pins.
Dear sir
I would rechecked it has 6 pins.
Out of 6 pins, 2 pins are not connected.
Remaining out of four, VCC, GND, Output and anthoer pin is through 8K ohms grounded
Please suggest me suitable IC Datasheet.
Hello pottenenir,
I was unable to find any match to the VJ part marking, with 6 leads.
Maybe Adam7 will have better luck.