Positioner head for DMC AF8 to crimp Amphenol Socapex M39029/58-360 Contacts

What positioner head do I need for my DMC AF8 to crimp Amphenol Socapex M39029/58-360 Contacts? I see a K42 for the AFM8, but don’t know if it is compatible with the AF8 as well.

Hello, Charles. Welcome to TechForum!

From the documentation I’m seeing on this product, M22520/2-09 is being called out as the pin contact positioner for this tool and contact type. The TE number should be compatible with standard tooling like the AF8 crimper, MIL specs keep these product types all generally interchangeable between suppliers.