LC29HCAMD do this come as a module
eg. mounted on board or just the gps chip shown in picture of this product like below?
Hello mr.yp1556,
The Quectel part number LC29HCAMD is actually a module board. We do not have this same gps chip mounted on a larger module board.
Hi mr.yp1556,
As @David_1768 stated, this is a module with multiple components soldered to a board and covered with a metal RF shield. This board is designed to be soldered down onto another base-board that the user creates.
If you are looking for a development board for that module, which presumably would not require any soldering, then the 2958-LC29HCAEK-ND is an option. Unfortunately, we do not have an image of it and one is required to register on the Quectel website before obtaining any information about it.
Screen shot of Quectel GNSS LC29H series product page
We do not stock the 2958-LC29HCAEK-ND eval board, but if the lead-time given to us is to be believed, an order today could get it here by the end of the month.
(Note: image is incorrect - image shown is just the module, not the whole Eval Board)
Additionally, we offer the following boards which use other Quectel modules from the LC29H family:
MIKROE-5933 GNSS RTK 3 CLICK - LC29HEA
MIKROE-5914 GNSS RTK 3 CLICK - LC29HDA