I am looking 2958-UMTS-LTEEVB-KIT-ND development board , i need to know this comes with GSM module EC25 E or should we buy module separately ?
if Separately need to order EC25 E module , pls share the Module details here
I am looking 2958-UMTS-LTEEVB-KIT-ND development board , i need to know this comes with GSM module EC25 E or should we buy module separately ?
if Separately need to order EC25 E module , pls share the Module details here
Hello embeddedtech - welcome to the Forum Community. This is the kit contents:
USB to UART converter cable x1
USB cable x1
RF cables x4
Main Antennas x2
GNSS Antenna (passive) x1
Wi-Fi Antenna x1
Earphone x1
USB 2.0 to RS232 driver and USB driver disk x1
ALC5616 and TLV320AIC3104 codec boards x2
Bolts and nuts for assembling EVB x1 (4 for each type)
Instruction sheet of giving instructions for EVB connection, details of EVB accessories, etc. x1
Applicable modules:
• UMTS & LTE Modules:
• UC20
• UGxx (UG96/UG95)
• EC2x (EC25/EC21/EC20/EC20 R2.0/EC20 R2.1)
• EG9x (EG91/EG95)
• AG35
• BG96
• Wi-Fi Modules:
• FC20 Series (FC20/FC20-N)
• AF20
Link to the details from the manufacturer’s website.
Hi @embeddedtech ,
The UMTS-LTEEVB-KIT does not include the module or test boards as those are user selectable. 2958-EC25EFATEA-512-STD-ND should work for you, please review datasheet specifications before ordering.
The “TEA” in the part number demonstrates the module is pre-mounted on the (daughter) board. Without the TEA it will be the surface mount module chip only.