Programming issues, with the Atmega32 controller

I have seceral brand new Atmega32a microprocessors, and I have boards already made, and programming started, and I cannot get it to read the chip ID. When I use any programer, it says the chip is ready to accept data, and then it exits, giving me the following error:

Arduino: 1.8.19 (Windows 7), Board: "ATmega32, No bootloader, EEPROM retained, Standard pinout, BOD 2.7V, LTO disabled, External 8 MHz"

C:\Program Files (x86)\Arduino\arduino-builder -dump-prefs -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\Kims\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\Kims\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Kims\Documents\Arduino\libraries -fqbn=MightyCore:avr:32:bootloader=no_bootloader,eeprom=keep,pinout=standard,BOD=2v7,LTO=Os,clock=8MHz_external -vid-pid=2341_0043 -ide-version=10819 -build-path C:\Users\Kims\AppData\Local\Temp\arduino_build_565344 -warnings=all -build-cache C:\Users\Kims\AppData\Local\Temp\arduino_cache_885821 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.avr-gcc.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7 -prefs=runtime.tools.avr-gcc-7.3.0-atmel3.6.1-arduino7.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7 -prefs=runtime.tools.avrdude.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino18 -prefs=runtime.tools.avrdude-6.3.0-arduino18.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino18 -prefs=runtime.tools.arduinoOTA.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.3.0 -prefs=runtime.tools.arduinoOTA-1.3.0.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.3.0 -verbose I:\1A CTC SIGNAL SCHEMATICS\CONTROL POINT FIRMWARE\RIGHT HAND TURNOUT CONTROL POINT\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino

C:\Program Files (x86)\Arduino\arduino-builder -compile -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\Kims\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\Kims\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Kims\Documents\Arduino\libraries -fqbn=MightyCore:avr:32:bootloader=no_bootloader,eeprom=keep,pinout=standard,BOD=2v7,LTO=Os,clock=8MHz_external -vid-pid=2341_0043 -ide-version=10819 -build-path C:\Users\Kims\AppData\Local\Temp\arduino_build_565344 -warnings=all -build-cache C:\Users\Kims\AppData\Local\Temp\arduino_cache_885821 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.avr-gcc.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7 -prefs=runtime.tools.avr-gcc-7.3.0-atmel3.6.1-arduino7.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avr-gcc\7.3.0-atmel3.6.1-arduino7 -prefs=runtime.tools.avrdude.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino18 -prefs=runtime.tools.avrdude-6.3.0-arduino18.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino18 -prefs=runtime.tools.arduinoOTA.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.3.0 -prefs=runtime.tools.arduinoOTA-1.3.0.path=C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\arduinoOTA\1.3.0 -verbose I:\1A CTC SIGNAL SCHEMATICS\CONTROL POINT FIRMWARE\RIGHT HAND TURNOUT CONTROL POINT\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino

Using board '32' from platform in folder: C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3

Using core 'MCUdude_corefiles' from platform in folder: C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3

Warning: Board ATmega32-Arduino-master:mega32:mega32-1 doesn't define a 'build.board' preference. Auto-set to: MEGA32_MEGA32-1

Warning: Board ATmega32-Arduino-master:mega32:mega32-8 doesn't define a 'build.board' preference. Auto-set to: MEGA32_MEGA32-8

Warning: Board ATmega32-Arduino-master:mega32:mega32-16 doesn't define a 'build.board' preference. Auto-set to: MEGA32_MEGA32-16

Warning: Board arduino:avr:mega32-8 doesn't define a 'build.board' preference. Auto-set to: AVR_MEGA32-8

Warning: Board arduino:avr:mega32-1 doesn't define a 'build.board' preference. Auto-set to: AVR_MEGA32-1

Warning: Board arduino:avr:mega32-16 doesn't define a 'build.board' preference. Auto-set to: AVR_MEGA32-16

Detecting libraries used...

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-g++" -c -g -Os -w -std=gnu++17 -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -w -x c++ -E -CC -mmcu=atmega32 -DF_CPU=8000000L -DARDUINO=10819 -DARDUINO_AVR_ATmega32 -DARDUINO_ARCH_AVR "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\cores\\MCUdude_corefiles" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\variants\\standard" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp" -o nul

Alternatives for Servo.h: [Servo@1.1.8 Servo@1.1.1]

ResolveLibrary(Servo.h)

  -> candidates: [Servo@1.1.8 Servo@1.1.1]

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-g++" -c -g -Os -w -std=gnu++17 -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -w -x c++ -E -CC -mmcu=atmega32 -DF_CPU=8000000L -DARDUINO=10819 -DARDUINO_AVR_ATmega32 -DARDUINO_ARCH_AVR "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\cores\\MCUdude_corefiles" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\variants\\standard" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\libraries\\Servo\\src" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp" -o nul

Using cached library dependencies for file: C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3\libraries\Servo\src\Servo.cpp

Generating function prototypes...

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-g++" -c -g -Os -w -std=gnu++17 -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -w -x c++ -E -CC -mmcu=atmega32 -DF_CPU=8000000L -DARDUINO=10819 -DARDUINO_AVR_ATmega32 -DARDUINO_ARCH_AVR "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\cores\\MCUdude_corefiles" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\variants\\standard" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\libraries\\Servo\\src" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp" -o "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\preproc\\ctags_target_for_gcc_minus_e.cpp"

"C:\\Program Files (x86)\\Arduino\\tools-builder\\ctags\\5.8-arduino11/ctags" -u --language-force=c++ -f - --c++-kinds=svpf --fields=KSTtzns --line-directives "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\preproc\\ctags_target_for_gcc_minus_e.cpp"

Compiling sketch...

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-g++" -c -g -Os -Wall -Wextra -std=gnu++17 -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -MMD -mmcu=atmega32 -DF_CPU=8000000L -DARDUINO=10819 -DARDUINO_AVR_ATmega32 -DARDUINO_ARCH_AVR "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\cores\\MCUdude_corefiles" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\variants\\standard" "-IC:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\MightyCore\\hardware\\avr\\2.1.3\\libraries\\Servo\\src" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp" -o "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp.o"

I:\1A CTC SIGNAL SCHEMATICS\CONTROL POINT FIRMWARE\RIGHT HAND TURNOUT CONTROL POINT\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino: In function 'void loop()':

I:\1A CTC SIGNAL SCHEMATICS\CONTROL POINT FIRMWARE\RIGHT HAND TURNOUT CONTROL POINT\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino:87:4: warning: 'pos' may be used uninitialized in this function [-Wmaybe-uninitialized]

    if(pos <= 116){

    ^~

Compiling libraries...

Compiling library "Servo"

Using previously compiled file: C:\Users\Kims\AppData\Local\Temp\arduino_build_565344\libraries\Servo\Servo.cpp.o

Compiling core...

Using precompiled core: C:\Users\Kims\AppData\Local\Temp\arduino_cache_885821\core\core_3a5f066219652446b24b40b2539c9d55.a

Linking everything together...

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-gcc" -Wall -Wextra -Os -Wl,--gc-sections,--section-start=.FAR_MEM1=0x10000 -mmcu=atmega32 -o "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.elf" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\sketch\\RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.cpp.o" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344\\libraries\\Servo\\Servo.cpp.o" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/..\\arduino_cache_885821\\core\\core_3a5f066219652446b24b40b2539c9d55.a" "-LC:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344" -lm

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-objcopy" -O ihex -j .eeprom --set-section-flags=.eeprom=alloc,load --no-change-warnings --change-section-lma .eeprom=0 "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.elf" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.eep"

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-objcopy" -O ihex -R .eeprom "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.elf" "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.hex"

cmd /C "C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-objdump" --disassemble --source --line-numbers --demangle --section=.text "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.elf" > "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino_atmega32_8000000L.lst"

Multiple libraries were found for "Servo.h"

 Used: C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3\libraries\Servo

 Not used: C:\Program Files (x86)\Arduino\libraries\Servo

Using library Servo at version 1.1.1 in folder: C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3\libraries\Servo 

"C:\\Users\\Kims\\AppData\\Local\\Arduino15\\packages\\arduino\\tools\\avr-gcc\\7.3.0-atmel3.6.1-arduino7/bin/avr-size" -A "C:\\Users\\Kims\\AppData\\Local\\Temp\\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.elf"

Sketch uses 2676 bytes (8%) of program storage space. Maximum is 32768 bytes.

Global variables use 52 bytes (2%) of dynamic memory, leaving 1996 bytes for local variables. Maximum is 2048 bytes.

C:\Users\Kims\AppData\Local\Arduino15\packages\arduino\tools\avrdude\6.3.0-arduino18/bin/avrdude -CC:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3/avrdude.conf -v -patmega32 -cstk500v1 -PCOM18 -b19200 -Uflash:w:C:\Users\Kims\AppData\Local\Temp\arduino_build_565344/RIGHT_HAND_TURNOUT_CONTROL_POINT_Firmware.ino.with_bootloader.hex:i 

avrdude: Version 6.3-20201216

         Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/

         Copyright (c) 2007-2014 Joerg Wunsch



         System wide configuration file is "C:\Users\Kims\AppData\Local\Arduino15\packages\MightyCore\hardware\avr\2.1.3/avrdude.conf"



         Using Port                    : COM18

         Using Programmer              : stk500v1

         Overriding Baud Rate          : 19200

         AVR Part                      : ATmega32

         Chip Erase delay              : 9000 us

         PAGEL                         : PD7

         BS2                           : PA0

         RESET disposition             : dedicated

         RETRY pulse                   : SCK

         serial program mode           : yes

         parallel program mode         : yes

         Timeout                       : 200

         StabDelay                     : 100

         CmdexeDelay                   : 25

         SyncLoops                     : 32

         ByteDelay                     : 0

         PollIndex                     : 3

         PollValue                     : 0x53

         Memory Detail                 :



                                  Block Poll               Page                       Polled

           Memory Type Mode Delay Size  Indx Paged  Size   Size #Pages MinW  MaxW   ReadBack

           ----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------

           eeprom         4    10    64    0 no       1024    4      0  9000  9000 0xff 0xff

           flash         33     6    64    0 yes     32768  128    256  4500  4500 0xff 0xff

           lfuse          0     0     0    0 no          1    0      0  2000  2000 0x00 0x00

           hfuse          0     0     0    0 no          1    0      0  2000  2000 0x00 0x00

           efuse          0     0     0    0 no          0    0      0     0     0 0x00 0x00

           lock           0     0     0    0 no          1    0      0  2000  2000 0x00 0x00

           signature      0     0     0    0 no          3    0      0     0     0 0x00 0x00

           calibration    0     0     0    0 no          4    0      0     0     0 0x00 0x00



         Programmer Type : STK500

         Description     : Atmel STK500 Version 1.x firmware

         Hardware Version: 2

         Firmware Version: 1.18

         Topcard         : Unknown

         Vtarget         : 0.0 V

         Varef           : 0.0 V

         Oscillator      : Off

         SCK period      : 0.1 us



avrdude: AVR device initialized and ready to accept instructions



Reading | ################################################## | 100% 0.02s



avrdude: Device signature = 0x000000 (retrying)



Reading | ################################################## | 100% 0.02s



avrdude: Device signature = 0x000000 (retrying)



An error occurred while uploading the sketch

Reading | ################################################## | 100% 0.02s



avrdude: Device signature = 0x000000

avrdude: Yikes!  Invalid device signature.

         Double check connections and try again, or use -F to override

         this check.





avrdude done.  Thank you.
```

I really need some help with this. I am 2 months behind in my product development, and I am completely stuck.

Thank you in advance, for all your help!!!

Taz...

Do you have an external voltage source supplied to the chip while you’re programming it?

Vtarget is coming back 0.0 V

Just for details, which “programmer” are you actually using, what wires do you have wired in and how is it and the device powered?

Regards,

No, but, I was able to upload normally last night. I used the Arduino as a ISP. It all of a sudden worked. I will still try to use the USBISP soon, and will try
that.

Thank you!!!

Hello, Robert!

I was able to get it to work last night late. I tried the Arduino, as the ISP, and used another, new breadboard. I was able to get it to upload.

Thank you!!! I will keep open this thread, as I may need further assistance, using the USBISP. I have 2 different ones, one uses the Attiny2313, and the other uses the Atmega88 or 8. I cannot get the the drivers to see it, although it DOES give me the connection sound when I plug them in. THAT is a problem, I will address in the next few days. I want to make sure, I can get the I/O’s working correctly. I am doing that at the moment.
Many Thanks folks. I wish I had known about this forum earlier. You’ve been a great help.

Blessings…

Taz…