PTFE TUBE KIT- 2.85MM .is it compatible with ultimaker 2+

PTFE TUBE KIT- 2.85MM .is it compatible with ultimaker 2+ 3D printer.

Hi,

The KT-MS0020 PTFE bowden tube replacement kit would work for the ultimaker 2+ as it utilizes 2.85mm filament. I had to check to make sure the length would be enough for that specific printer which requires about 705mm and this kit is 800mm so you may have to trim it a bit but it will work

dear,

What’s the OD & ID of the tube.

will I get 02 collets and 02 clips with the PTFE tube.

Hello,
I sent a request to the manufacturer for this information and will post when I get it.

Here is the information provided by the manufacturer.

These are the Feed Tube, 0.187" ID X .250" OD NAT PTFE Tube.

Please reply

Looking at the manufacturer website it appears that collets and clips are not included.

Parts Included

One (1) x 800 mm length 2.85 mm diameter PTFE Tube