Hello, this is my first post, I would like to operate 1 light using a 12 volt regulated DC power supply from 4 switches. I would like to be able to turn the light on or off from any switch. I have been given a relay # from Verna Nelson part # 255-1739-ND. Being a rookie to electronics I would like to know if it is possible to get directions on how to make the connections. I have 4 N/O and 4 N/C switches, could these be used or do I need different switches. Any and al info would be greatly appreciated. Thank You
Greetings,
Control of a single load via multiple switches is known as multi-way switching. Simple SPST switches of either flavor are not suitable for this purpose; SPDT and/or DPDT types are required depending on the desired number of switches in the circuit.