RT curves. where are they?

------Question for NCU15XH103D6SRC Please Put your question below------

The published data sheet for NCU15XH103D6SRC has an RT curve in the form of a small chart. I need to get the data in table form for it to actually be useful. Preferably one table for each beta, i.e. B25/85). I was unable to locate such information on the website. Can i request this info be sent to me? or give me link? Thanks!

https://www.murata.com/products/productdata/8798887739422/NTHCG272.txt?1743059744000

  
                                              NC-R4066

    P/N     NCU15XH103D6SRC
    R25          10      k ohm +/-      0.5          %
  B(25/50)      3380       K +/-        0.5          %

   TEMP.       R-low      R-center     R-high
  (deg.C)     (k ohm)     (k ohm)     (k ohm)
    -55       450.0335    461.0419    472.3079
    -54       425.3940    435.6765    446.1963
    -53       402.0822    411.6846    421.5058
    -52       380.0331    388.9987    398.1658
    -51       359.1841    367.5536    376.1087
    -50       339.4750    347.2867    355.2693
    -49       320.8480    328.1380    335.5853
    -48       303.2476    310.0498    316.9966
    -47       286.6207    292.9669    299.4461
    -46       270.9164    276.8365    282.8789
    -45       256.0862    261.6082    267.2425
    -44       242.0836    247.2337    252.4872
    -43       228.8643    233.6673    238.5652
    -42       216.3862    220.8651    225.4311
    -41       204.6090    208.7854    213.0418
    -40       193.4940    197.3881    201.3556
    -39       182.9072    186.5355    190.2310
    -38       172.9723    176.3540    179.7974
    -37       163.6450    166.7979    170.0073
    -36       154.8841    157.8245    160.8168
    -35       146.6515    149.3947    152.1854
    -34       138.9471    141.5077    144.1120
    -33       131.6979    134.0889    136.5199
    -32       124.8743    127.1074    129.3772
    -31       118.4487    120.5349    122.6547
    -30       112.3952    114.3446    116.3250
    -29       106.7049    108.5273    110.3780
    -28       101.3386    103.0426    104.7727
    -27       96.2759     97.8696     99.4872
    -26       91.4978     92.9886     94.5013
    -25       86.9865     88.3814     89.7963
    -24       82.7307     84.0361     85.3600
    -23       78.7091     79.9311     81.1700
    -22       74.9075     76.0515     77.2111
    -21       71.3126     72.3838     73.4692
    -20       67.9118     68.9150     69.9312
    -19       64.6943     65.6339     66.5856
    -18       61.6484     62.5287     63.4199
    -17       58.7640     59.5887     60.4235
    -16       56.0315     56.8043     57.5863
    -15       53.4422     54.1664     54.8990
    -14       50.9867     51.6654     52.3518
    -13       48.6583     49.2944     49.9376
    -12       46.4498     47.0461     47.6488
    -11       44.3543     44.9132     45.4781
    -10       42.3653     42.8893     43.4187
     -9       40.4756     40.9668     41.4630
     -8       38.6810     39.1416     39.6066
     -7       36.9763     37.4080     37.8439
     -6       35.3563     35.7611     36.1696
     -5       33.8165     34.1960     34.5789
     -4       32.3512     32.7069     33.0658
     -3       30.9576     31.2912     31.6275
     -2       29.6320     29.9446     30.2598
     -1       28.3705     28.6636     28.9590
     0        27.1698     27.4445     27.7213
     1        26.0256     26.2831     26.5424
     2        24.9360     25.1773     25.4203
     3        23.8981     24.1242     24.3518
     4        22.9092     23.1210     23.3342
     5        21.9666     22.1650     22.3647
     6        21.0674     21.2532     21.4402
     7        20.2100     20.3840     20.5590
     8        19.3922     19.5551     19.7189
     9        18.6119     18.7644     18.9177
     10       17.8674     18.0101     18.1534
     11       17.1563     17.2897     17.4238
     12       16.4774     16.6022     16.7276
     13       15.8291     15.9458     16.0629
     14       15.2098     15.3188     15.4283
     15       14.6181     14.7199     14.8222
     16       14.0524     14.1475     14.2430
     17       13.5117     13.6005     13.6895
     18       12.9947     13.0775     13.1606
     19       12.5003     12.5775     12.6549
     20       12.0274     12.0993     12.1714
     21       11.5748     11.6418     11.7089
     22       11.1416     11.2040     11.2664
     23       10.7271     10.7850     10.8431
     24       10.3301     10.3840     10.4379
     25        9.9500     10.0000     10.0500
     26        9.5823      9.6323      9.6822
     27        9.2301      9.2800      9.3299
     28        8.8928      8.9425      8.9922
     29        8.5695      8.6190      8.6685
     30        8.2597      8.3089      8.3582
     31        7.9628      8.0117      8.0606
     32        7.6781      7.7266      7.7753
     33        7.4051      7.4532      7.5015
     34        7.1432      7.1909      7.2388
     35        6.8919      6.9392      6.9867
     36        6.6508      6.6977      6.7447
     37        6.4195      6.4658      6.5123
     38        6.1973      6.2432      6.2892
     39        5.9840      6.0293      6.0748
     40        5.7792      5.8239      5.8689
     41        5.5824      5.6266      5.6711
     42        5.3934      5.4370      5.4809
     43        5.2117      5.2548      5.2981
     44        5.0371      5.0796      5.1223
     45        4.8692      4.9111      4.9532
     46        4.7078      4.7491      4.7906
     47        4.5525      4.5933      4.6342
     48        4.4032      4.4433      4.4837
     49        4.2595      4.2990      4.3388
     50        4.1212      4.1601      4.1993
     51        3.9881      4.0265      4.0650
     52        3.8600      3.8977      3.9357
     53        3.7367      3.7738      3.8112
     54        3.6178      3.6544      3.6912
     55        3.5034      3.5393      3.5755
     56        3.3931      3.4285      3.4641
     57        3.2869      3.3216      3.3567
     58        3.1845      3.2187      3.2531
     59        3.0857      3.1194      3.1533
     60        2.9906      3.0236      3.0570
     61        2.8988      2.9313      2.9641
     62        2.8103      2.8422      2.8744
     63        2.7249      2.7563      2.7879
     64        2.6425      2.6733      2.7045
     65        2.5630      2.5933      2.6239
     66        2.4862      2.5160      2.5461
     67        2.4121      2.4414      2.4710
     68        2.3406      2.3694      2.3984
     69        2.2716      2.2998      2.3284
     70        2.2048      2.2326      2.2606
     71        2.1404      2.1677      2.1952
     72        2.0781      2.1049      2.1320
     73        2.0180      2.0443      2.0709
     74        1.9598      1.9857      2.0118
     75        1.9036      1.9290      1.9547
     76        1.8493      1.8742      1.8994
     77        1.7968      1.8213      1.8460
     78        1.7460      1.7700      1.7943
     79        1.6968      1.7204      1.7443
     80        1.6493      1.6725      1.6959
     81        1.6033      1.6261      1.6491
     82        1.5588      1.5812      1.6038
     83        1.5158      1.5377      1.5599
     84        1.4741      1.4956      1.5175
     85        1.4337      1.4549      1.4763
     86        1.3947      1.4155      1.4365
     87        1.3569      1.3773      1.3979
     88        1.3202      1.3403      1.3606
     89        1.2848      1.3044      1.3244
     90        1.2504      1.2697      1.2893
     91        1.2171      1.2361      1.2553
     92        1.1848      1.2035      1.2224
     93        1.1536      1.1719      1.1904
     94        1.1233      1.1412      1.1595
     95        1.0939      1.1115      1.1294
     96        1.0654      1.0828      1.1003
     97        1.0378      1.0548      1.0721
     98        1.0111      1.0278      1.0447
     99        0.9851      1.0015      1.0182
    100        0.9599      0.9760      0.9924
    101        0.9355      0.9513      0.9674
    102        0.9118      0.9274      0.9432
    103        0.8888      0.9041      0.9196
    104        0.8665      0.8815      0.8968
    105        0.8449      0.8596      0.8746
    106        0.8239      0.8384      0.8531
    107        0.8035      0.8177      0.8322
    108        0.7837      0.7977      0.8119
    109        0.7645      0.7782      0.7922
    110        0.7458      0.7593      0.7730
    111        0.7277      0.7410      0.7544
    112        0.7101      0.7231      0.7364
    113        0.6931      0.7058      0.7188
    114        0.6764      0.6890      0.7018
    115        0.6603      0.6726      0.6852
    116        0.6447      0.6568      0.6691
    117        0.6294      0.6414      0.6535
    118        0.6146      0.6264      0.6383
    119        0.6003      0.6118      0.6235
    120        0.5863      0.5976      0.6091
    121        0.5727      0.5838      0.5951
    122        0.5595      0.5704      0.5815
    123        0.5467      0.5574      0.5683
    124        0.5342      0.5447      0.5555
    125        0.5220      0.5324      0.5430
    126        0.5102      0.5204      0.5308
    127        0.4987      0.5088      0.5190
    128        0.4876      0.4974      0.5075
    129        0.4767      0.4864      0.4962
    130        0.4661      0.4756      0.4853
    131        0.4558      0.4652      0.4747
    132        0.4458      0.4550      0.4644
    133        0.4360      0.4451      0.4543
    134        0.4265      0.4354      0.4445
    135        0.4173      0.4260      0.4350
    136        0.4082      0.4169      0.4257
    137        0.3995      0.4080      0.4166
    138        0.3909      0.3993      0.4078
    139        0.3826      0.3908      0.3992
    140        0.3745      0.3826      0.3908
    141        0.3666      0.3745      0.3826
    142        0.3589      0.3667      0.3747
    143        0.3514      0.3590      0.3669
    144        0.3440      0.3516      0.3593
    145        0.3369      0.3443      0.3519
    146        0.3299      0.3372      0.3447
    147        0.3231      0.3303      0.3377
    148        0.3165      0.3236      0.3308
    149        0.3100      0.3170      0.3241
    150        0.3037      0.3106      0.3176

Data above is available from the manufacturer’s product page.

Note also that the SimSurfing utility just below that can provide substantial additional information, based on a model of the specific circuit used.

1 Like

Hi Rick and Kristof,
Thank you! Yes i found it right after i posted my question. Naturally, i would not have found it if i didn’t ask. The table isn’t in a very friendly format. csv would be nice.

Are there any other RT tables available? Specifically interested in the B25/85 and B25/100.

Only the B(25/50) is available.

Saving as a .txt and using the Excel text import can get a person there in a matter of seconds.

Also, the SimSurfing tool mentioned above can export in spreadsheet formats.

That’s the sort of question a person should ask carefully. Understand that beta values are something of a quick & dirty approximation that can be generated or transposed mathematically, and the tables derived from various temperature points are simply smearing the errors in the approximation around differently. It’s not always obvious whether any given table one might come across is a tabulation of values per the approximation, or a representation of part behavior.

It’s a territory where one can easily go off into the weeds on either side of the road, wasting time on things that don’t actually matter or neglecting to account for things that do…

1 Like