We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I am looking for a special type of circuit breaker. It needs to have 3 poles ja current rating up to 63A. I want to be able to open (only open, not closing) the circuit breaker connections as part of a safety circuit.
Otherwise the breaker would act like a normal circuit breaker. Add on is that I want to be able to trigger it OFF also remotely. It has to be some type of eFuse but I haven’t been able to find a suitable candidate. Contactor is not the answer in this case It would do the job yes but I want to know does this type of circuit breaker exist?
Also a circuit breaker is a safety device, as such it should never be used to do anything but break a circuit when the current limit is exceeded. So adding any kind of remote control capability is an extreme violation of pretty much all global safety standards.
The missing term in this conversation is “shunt trip.”
The shunt trip is an option that allows a circuit breaker to be remotely tripped by an auxiliary system. For example, a large 63 A 3-phase circuit breaker may be tripped by applying a 24 VDC signal to the shunt trip circuit.
One option is this circuit breaker manufactured by Phoenix Contact:
We need to carefully examine the datasheet to find the part number for the shunt trip accessory. Note that the several different versions are available with a voltage rating to match your system. One example is this 24 VDC side mount accessor is located here:
This picture shows how the shunt trip is installed on the side of the larger circuit breaker.
Welcome to the DigiKey community. Please let us know how you solved the problem.