Hi! I mistakenly ordered (5) SemiTec NTC Thermistors (PN: 4316-103AT-11ND) and realized that the lead wire was much too short for its intended use (sensor replacement in an Accucold ACR1718RH-MED fridge). The fridge’s current sensor’s lead wire measures approx 10FT. I tried to locate the exact same sensor and thought I had found the correct replacement, but this product is only 23.03". Any chance I can return and get custom length wires (if this wire length is not already offered)? Thanks!
Hello H_Cal,
Welcome to the DigiKey TechForum.
You can return the items, by contacting Customer.Resolution@DigiKey.com
We do not have a perfect match, with about a 10’ length of wire.
CLICK HERE for the closest options we have available. The wire lengths of these range from 116.56” to 196.85”.
Please check the datasheets to determine compatibility to your application.