Hello Paul, I have taken on a small project of adding a USB-C port to a cup holder in my car using the 1568-1958-ND -Sparkfun USB-C Breakout Board and cannot get it to provide the 5V, 3A output for charging a phone. I’ve tried several methods including the 5.1K ohm resistors, and also a DC-DC 12V in/ 5V 3A output at the USB-C board, and the phone won’t recognize the power source. Can you offer some advice…I’m a novice at best.
Related topics
Topic | Replies | Views | Activity | |
---|---|---|---|---|
Need product advice for a DC TO TYPE-C ADAPTER | 4 | 360 | November 1, 2023 | |
Default USB Type-C Output Expectations | 12 | 1766 | December 21, 2023 | |
USB PD out to 24V@3A DC | 6 | 515 | December 23, 2023 | |
Cable to ensure max draw of 3A over USB | 7 | 792 | November 10, 2023 | |
Need some help on USB PD providing 5v 3amps output | 1 | 648 | April 25, 2021 |