In our previous article, we explored the fundamentals of parallel battery charging, explaining how configuring batteries in parallel increases capacity and extends battery life. Now that we understand the basics, let’s dive into how USB-C technology takes parallel charging to the next level.
USB-C ports are becoming the standard for consumer devices because they offer much more flexibility than previous USB ports. Among the key benefits driving their popularity are higher power delivery and longer battery life. As a result, the need to charge devices at higher power levels is becoming increasingly important. This article will cover the integration, benefits, and drawbacks of parallel battery charging and USB-C in the consumer market.
USB-C’s Integration into Modern Parallel Battery Charging
As mentioned earlier, USB-C ports and devices have the ability to be charged at higher power levels compared to previous USB 2.0 and USB 3.0.
The most recent version of the USB-C spec, Power Delivery 3.1, can deliver up to 240 W, While this may be more than most consumer products require, it highlights the increased robustness of USB-C technology.
Example: Analog Devices’ MAX77958 is a USB-C PD controller that handles PD 3.0 negotiation, cable detection, and even drives external chargers—making it ideal for smart, dynamic power distribution in parallel battery charging systems.
More Power, More Performance
As the battery capacity of a consumer device increases due to the parallel battery configuration, so does the power requirement for the charger supplying power to the device.
The higher power from USB-C ports allows consumers to charge their device faster than before and results in more time for them to use the device, without the attachment to a charging cable.
Benefits and Drawbacks
Parallel battery charging with USB-C has already made its way into many applications and will continue to spread throughout consumer applications.
While USB-C ports and cables will be largely beneficial to the consumer market in terms of power, cost, and simplicity, there are some drawbacks that need to be pointed out.
Table 1. Benefits of USB-C and Parallel Battery Charging
Today’s consumers want long battery life and less time tethered to a charger. USB-C helps make this possible with:
| Single cable | Power and data are on the same cable, which is beneficial in space constrained applications |
| High power levels | Increased capacity and higher charging levels allow for a larger range of possible applications, including both low power consumer devices and high power tools and computers |
| Time savings | The high charge current capabilities of USB-C allow for charging batteries in parallel, which results in more usable capacity in the amount of time it takes to charge just one battery |
| Simple integration | A USB-C cable is reversible and can be plugged in either way, while adding additional batteries in parallel simply requires connecting the power source to the terminals of the new battery |
| Reduced electronic waste over time | Using a common USB-C charger for multiple devices would reduce electronic waste around the world |
Table 2. Drawbacks of USB-C and Parallel Battery Charging
Despite all the benefits, there are a few challenges when combining USB-C and parallel battery charging:
| Differences in ports | Complications over power levels can occur if both ports do not match. The multiple ports include Thunderbolt, Power Delivery 3.1, and Power Delivery 3.0 |
| More expensive | Additional batteries along with ports and cables that allow for faster charging require advanced technology, which is more expensive than previous versions |
| Cable replacement | New USB-C cables will force USB-A, USB-B, and micro-USB cables to be replaced and the older cables will become obsolete |
| Larger size | Adding an additional battery is going to take up extra space, which can become an issue in applications where size is a critical specification |
| Increased complexity | Including an additional battery introduces a few complex issues, such as the need to balance aging across the batteries and ensuring charge cycles begin at similar voltages so the batteries or wiring is not damaged |
USB Type-C® Power Delivery Connectors
What’s Next?
So far, we’ve discussed the basics of parallel battery charging and how USB-C enhances its performance. But how does this all work in the real world? Check out our next article: “Real-World Applications and Design Tips”
Related Article
Parallel Battery Charging – and Why Does It Matter?
Implementing USB-C Parallel Charging Systems with MAX17330
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| 175-MAX17262HEWL+TTR-ND,175-MAX17262HEWL+TCT-ND,175-MAX17262HEWL+TDKR-ND | MAX17262HEWL+T |
| 175-MAX17260SEWL+TTR-ND,175-MAX17260SEWL+TCT-ND,175-MAX17260SEWL+TDKR-ND | MAX17260SEWL+T |
| 175-MAX17262REWL+TTR-ND,175-MAX17262REWL+TCT-ND,175-MAX17262REWL+TDKR-ND | MAX17262REWL+T |
| 505-MAX17260SETD±ND | MAX17260SETD+ |
| 175-MAX17260SETD+TTR-ND,175-MAX17260SETD+TCT-ND,175-MAX17260SETD+TDKR-ND | MAX17260SETD+T |
| MAX17048G+T10TR-ND,MAX17048G+T10CT-ND,MAX17048G+T10DKR-ND | MAX17048G+T10 |
| MAX17055EWL+TTR-ND,MAX17055EWL+TCT-ND,MAX17055EWL+TDKR-ND | MAX17055EWL+T |
| MAX17055ETB+TTR-ND,MAX17055ETB+TCT-ND,MAX17055ETB+TDKR-ND | MAX17055ETB+T |
| 175-MAX17303X+TTR-ND,175-MAX17303X+TCT-ND,175-MAX17303X+TDKR-ND | MAX17303X+T |
| MAX17201G+TTR-ND,MAX17201G+TCT-ND,MAX17201G+TDKR-ND | MAX17201G+T |
| 175-MAX17261METD+TTR-ND,175-MAX17261METD+TCT-ND,175-MAX17261METD+TDKR-ND | MAX17261METD+T |
| MAX17261METD±ND | MAX17261METD+ |
| MAX6778XK+TTR-ND,MAX6778XK+TCT-ND,MAX6778XK+TDKR-ND | MAX6778XK+T |
| MAX17201G±ND | MAX17201G+ |
| MAX17205G+00E-ND | MAX17205G+00E |
| MAX17205G+TTR-ND,MAX17205G+TCT-ND,MAX17205G+TDKR-ND | MAX17205G+T |
| 175-MAX17330X22+TTR-ND,175-MAX17330X22+TCT-ND,175-MAX17330X22+TDKR-ND | MAX17330X22+T |
| DS2745U+TR-ND,DS2745U+CT-ND,DS2745U+DKR-ND | DS2745U+T&R |
| 175-DS2786G+T&RTR-ND,175-DS2786G+T&RCT-ND,175-DS2786G+T&RDKR-ND | DS2786G+T&R |
| 175-DS2782E+T&RTR-ND,175-DS2782E+T&RCT-ND,175-DS2782E+T&RDKR-ND | DS2782E+T&R |
| 175-MAX38888ATD+TTR-ND,175-MAX38888ATD+TCT-ND,175-MAX38888ATD+TDKR-ND | MAX38888ATD+T |
| DS2438Z+T&RTR-ND,DS2438Z+T&RCT-ND,DS2438Z+T&RDKR-ND | DS2438Z+T&R |
| 175-DS2788E+T&RTR-ND,175-DS2788E+T&RCT-ND,175-DS2788E+T&RDKR-ND | DS2788E+T&R |
| DS2788E±ND | DS2788E+ |
| DS2777G±ND | DS2777G+ |
| 175-MAX14680EWC+TTR-ND,175-MAX14680EWC+TCT-ND,MAX14680EWC+TCT-ND,175-MAX14680EWC+TDKR-ND | MAX14680EWC+T |
| 175-MAX17048X+T10TR-ND,175-MAX17048X+T10CT-ND,175-MAX17048X+T10DKR-ND | MAX17048X+T10 |
| 175-MAX17260BEWL+TTR-ND,175-MAX17260BEWL+TCT-ND,175-MAX17260BEWL+TDKR-ND | MAX17260BEWL+T |
| MAX6776XKC+TR-ND,MAX6776XKC+CT-ND,MAX6776XKC+DKR-ND | MAX6776XKC+T |
| MAX6775XKB+TTR-ND,MAX6775XKB+TCT-ND,MAX6775XKB+TDKR-ND | MAX6775XKB+T |
| 505-MAX17303G±ND | MAX17303G+ |
| MAX17201G+00E-ND | MAX17201G+00E |
| MAX6777XK+TR-ND,MAX6777XK+CT-ND,MAX6777XK+DKR-ND | MAX6777XK+T |
| 505-MAX17320G20±ND | MAX17320G20+ |
| 505-MAX17320G22±ND | MAX17320G22+ |
| MAX17205G±ND | MAX17205G+ |
| 175-MAX17301X+TTR-ND,175-MAX17301X+TCT-ND,175-MAX17301X+TDKR-ND | MAX17301X+T |
| DS2745U±ND | DS2745U+ |
| DS2782G±ND | DS2782G+ |
| 175-DS2756E+T&RTR-ND,175-DS2756E+T&RCT-ND,175-DS2756E+T&RDKR-ND | DS2756E+T&R |
| DS2756E±ND | DS2756E+ |
| DS2438AZ+TR-ND,DS2438AZ+CT-ND,DS2438AZ+DKR-ND | DS2438AZ+T&R |
| DS2438Z±ND | DS2438Z+ |
| 505-MAX17841BGUE/V±ND | MAX17841BGUE/V+ |
| DS2782E±ND | DS2782E+ |
| DS2764AE±ND | DS2764AE+ |
| DS2780E±ND | DS2780E+ |
| 175-DS2762AE+T&RTR-ND,175-DS2762AE+T&RCT-ND,175-DS2762AE+T&RDKR-ND | DS2762AE+T&R |
| MAX20303BEWN+TTR-ND,MAX20303BEWN+TCT-ND,MAX20303BEWN+TDKR-ND | MAX20303BEWN+T |
| MAX17843ACB/V±ND | MAX17843ACB/V+ |
| 175-MAX14634EWC+TTR-ND,175-MAX14634EWC+TCT-ND,175-MAX14634EWC+TDKR-ND | MAX14634EWC+T |
| MAX16915AUB±ND | MAX16915AUB+ |
| MAX16914AUB±ND | MAX16914AUB+ |
| 175-MAX17261MEWL+TTR-ND,175-MAX17261MEWL+TCT-ND,175-MAX17261MEWL+TDKR-ND | MAX17261MEWL+T |
| 175-MAX17201X+TTR-ND,175-MAX17201X+TCT-ND,175-MAX17201X+TDKR-ND | MAX17201X+T |
| MAX17215G+00E-ND | MAX17215G+00E |
| 175-MAX17320X20+TTR-ND,175-MAX17320X20+TCT-ND,175-MAX17320X20+TDKR-ND | MAX17320X20+T |
| MAX6775XKC+TTR-ND,MAX6775XKC+TCT-ND,MAX6775XKC+TDKR-ND | MAX6775XKC+T |
| 175-MAX6775XKA+TTR-ND,175-MAX6775XKA+TCT-ND,175-MAX6775XKA+TDKR-ND | MAX6775XKA+T |
| DS2786BG±ND | DS2786BG+ |
| 505-MAX17320G10±ND | MAX17320G10+ |
| 175-MAX6433UK+TTR-ND,175-MAX6433UK+TCT-ND,175-MAX6433UK+TDKR-ND | MAX6433UK+T |
| DS2746G±ND | DS2746G+ |
| MAX14653EWC+TTR-ND,MAX14653EWC+TCT-ND,MAX14653EWC+TDKR-ND | MAX14653EWC+T |
| 505-MAX17320G12±ND | MAX17320G12+ |
| DS2786G±ND | DS2786G+ |
| DS2781E+TR-ND,DS2781E+CT-ND,DS2781E+DKR-ND | DS2781E+T&R |
| DS2781G±ND | DS2781G+ |
| DS2438AZ±ND | DS2438AZ+ |
| DS2764BE±ND | DS2764BE+ |
| DS2778G±ND | DS2778G+ |
| DS2776G±ND | DS2776G+ |
| DS2781E±ND | DS2781E+ |
| DS2762BE±ND | DS2762BE+ |
| DS2762AE±ND | DS2762AE+ |
| MAX14920ECB±ND | MAX14920ECB+ |
| MAX14921ECS±ND | MAX14921ECS+ |
| 505-MAX17823BGCB/V±ND | MAX17823BGCB/V+ |
| 175-MAX14921ECS+TTR-ND,175-MAX14921ECS+TCT-ND,175-MAX14921ECS+TDKR-ND | MAX14921ECS+T |
| 175-MAX14670EWL+TTR-ND,175-MAX14670EWL+TCT-ND,175-MAX14670EWL+TDKR-ND | MAX14670EWL+T |
| MAX14606EWL+TTR-ND,MAX14606EWL+TCT-ND,MAX14606EWL+TDKR-ND | MAX14606EWL+T |
| 175-MAX6776XKB+TTR-ND,175-MAX6776XKB+TCT-ND,175-MAX6776XKB+TDKR-ND | MAX6776XKB+T |
| 175-MAX6776XKA+TTR-ND,175-MAX6776XKA+TCT-ND,175-MAX6776XKA+TDKR-ND | MAX6776XKA+T |
| MAX6775LTA+TTR-ND,MAX6775LTA+TCT-ND,MAX6775LTA+TDKR-ND,2156-MAX6775LTA+T-ND | MAX6775LTA+T |
| MAX17211G+00E-ND | MAX17211G+00E |
| MAX6436UT+TTR-ND,MAX6436UT+TCT-ND,MAX6436UT+TDKR-ND | MAX6436UT+T |
| 175-MAX6434UK+TTR-ND,175-MAX6434UK+TCT-ND,175-MAX6434UK+TDKR-ND | MAX6434UK+T |
| 175-MAX17215G+TTR-ND,175-MAX17215G+TCT-ND,175-MAX17215G+TDKR-ND | MAX17215G+T |
| DS2782G+TR-ND,DS2782G+CT-ND,DS2782G+DKR-ND | DS2782G+T&R |
| MAX1538ETI+TR-ND,MAX1538ETI+CT-ND,MAX1538ETI+DKR-ND | MAX1538ETI+T |
| 175-MAX17841BGUE/V+TTR-ND,175-MAX17841BGUE/V+TCT-ND,175-MAX17841BGUE/V+TDKR-ND | MAX17841BGUE/V+T |
| MAX1538ETI±ND | MAX1538ETI+ |
| DS2780G±ND | DS2780G+ |
| MAX1259CWE±ND | MAX1259CWE+ |
| 175-MAX14920ECB+TTR-ND,175-MAX14920ECB+TCT-ND,175-MAX14920ECB+TDKR-ND | MAX14920ECB+T |
| 505-MAX17853ACB/V±ND | MAX17853ACB/V+ |
| 175-MAX17823BGCB/V+TTR-ND,175-MAX17823BGCB/V+TCT-ND,175-MAX17823BGCB/V+TDKR-ND | MAX17823BGCB/V+T |
| 505-MAX17300G±ND | MAX17300G+ |
| 505-MAX17310G±ND | MAX17310G+ |
| MAX17215G±ND | MAX17215G+ |
| 175-MAX77972EWX+TTR-ND,175-MAX77972EWX+TCT-ND,175-MAX77972EWX+TDKR-ND | MAX77972EWX+T |
| 175-MAX14525ETA+TTR-ND,175-MAX14525ETA+TCT-ND,175-MAX14525ETA+TDKR-ND | MAX14525ETA+T |
| 505-MAX20095ATIA/VY±ND | MAX20095ATIA/VY+ |
| 505-MAX17330X22±ND | MAX17330X22+ |
| 505-MAX17301G±ND | MAX17301G+ |
| 505-MAX17841BGUE±ND | MAX17841BGUE+ |
| 505-ADES1756GCB/V±ND | ADES1756GCB/V+ |
| 505-MAX1259CPE±ND | MAX1259CPE+ |
| 505-ADES1755GCB/V±ND | ADES1755GCB/V+ |
| 505-ADES1754GCB/V±ND | ADES1754GCB/V+ |
| 505-MAX17823BGCB±ND | MAX17823BGCB+ |
| MAX17830GUN±ND | MAX17830GUN+ |
| MAX17830GUN/V±ND | MAX17830GUN/V+ |
| 175-MAX17830GUN/V+TTR-ND,175-MAX17830GUN/V+TCT-ND,175-MAX17830GUN/V+TDKR-ND | MAX17830GUN/V+T |
| 2156-MAX1707ETG±ND | MAX1707ETG+ |
| 2156-MAX6787TA±ND | MAX6787TA+ |
| 2156-MAX1786EUI±ND | MAX1786EUI+ |
| 2156-MAX17130ETL±ND | MAX17130ETL+ |
| 2156-MAX1786AEUI+T-ND | MAX1786AEUI+T |
| 2156-MAX8629ETI+T-ND | MAX8629ETI+T |
| 2156-MAX8618ETL±ND | MAX8618ETL+ |
| 2156-MAX8617ETL±ND | MAX8617ETL+ |
| 2156-MAX6781LTC±ND | MAX6781LTC+ |
| 2156-MAX1906VEGE-ND | MAX1906VEGE |
| 2156-MAX1906SEGE-ND | MAX1906SEGE |
| 2156-MAX6789TB±ND | MAX6789TB+ |
| 2156-MAX6790TB±ND | MAX6790TB+ |
| 2156-MAX4921BETD±ND | MAX4921BETD+ |
| 2156-MAX4920BETD±ND | MAX4920BETD+ |
| 2156-MAX6428ORUR±ND | MAX6428ORUR+ |
| 2156-MAX6428MQUR±ND | MAX6428MQUR+ |
| 2156-MAX6427DHUR-ND | MAX6427DHUR |
| 2156-MAX6436UT-T-ND | MAX6436UT-T |
| 2156-MAX6438UT-T-ND | MAX6438UT-T |
| 2156-MAX6431EHUS-T-ND | MAX6431EHUS-T |
| 2156-MAX6431FJUS-T-ND | MAX6431FJUS-T |
| 2156-MAX6432EIUS-T-ND | MAX6432EIUS-T |
| 2156-MAX6431CIUS-T-ND | MAX6431CIUS-T |
| 2156-MAX6431DHUS-T-ND | MAX6431DHUS-T |
| 2156-MAX6431CHUS-T-ND | MAX6431CHUS-T |
| 2156-MAX6432DHUS-T-ND | MAX6432DHUS-T |
| 2156-MAX6430ORUS-T-ND | MAX6430ORUS-T |
| 2156-MAX6432FJUS-T-ND | MAX6432FJUS-T |
| 2156-MAX6430EGUS-T-ND | MAX6430EGUS-T |
| 2156-MAX6432MRUS-T-ND | MAX6432MRUS-T |
| 2156-MAX6432EHUS-T-ND | MAX6432EHUS-T |
| 2156-MAX6430PQUS-T-ND | MAX6430PQUS-T |
| 2156-MAX6432ORUS-T-ND | MAX6432ORUS-T |
| 2156-MAX8629CETI±ND | MAX8629CETI+ |
| 2156-MAX1829ETL±ND | MAX1829ETL+ |
| 2156-MAX6429DHUR-T-ND | MAX6429DHUR-T |
| 2156-MAX6429MRUR-T-ND | MAX6429MRUR-T |
| 2156-MAX6427EHUR-T-ND | MAX6427EHUR-T |
| 2156-MAX6428AGUR-T-ND | MAX6428AGUR-T |
| 2156-MAX6429KTUR-T-ND | MAX6429KTUR-T |
| 2156-MAX6428MRUR-T-ND | MAX6428MRUR-T |
| 2156-MAX6427KQUR-T-ND | MAX6427KQUR-T |
| 2156-MAX6429EHUR-T-ND | MAX6429EHUR-T |
| 2156-MAX6429ORUR-T-ND | MAX6429ORUR-T |
| 2156-MAX6429EIUR-T-ND | MAX6429EIUR-T |
| 2156-MAX6786TA±ND | MAX6786TA+ |
| 2156-MAX6788TA±ND | MAX6788TA+ |
| 2156-MAX6847KASD3-ND | MAX6847KASD3 |
| 2156-MAX6440UTEHRD3-ND | MAX6440UTEHRD3 |
| 2156-MAX6847KARD3-T-ND | MAX6847KARD3-T |
| 2156-MAX6440UTEHRD3-T-ND | MAX6440UTEHRD3-T |
| 2156-MAX6847KASD3-T-ND | MAX6847KASD3-T |
| 2156-MAX6846KAWD3-T-ND | MAX6846KAWD3-T |
| 2156-MAX6440UTFJTD7-T-ND | MAX6440UTFJTD7-T |
| 2156-MAX6440UTKQSD3-T-ND | MAX6440UTKQSD3-T |
| 2156-MAX6439UTDHSD3-T-ND | MAX6439UTDHSD3-T |
| 2156-MAX17817EUI+T-ND | MAX17817EUI+T |
| 2156-MAX6849KAVD7-T-ND | MAX6849KAVD7-T |
| 2156-MAX6848KARD7-T-ND | MAX6848KARD7-T |
| 2156-MAX6849KASD3-T-ND | MAX6849KASD3-T |
| 2156-MAX6848KATD3-T-ND | MAX6848KATD3-T |
| 2156-MAX1827ETL-ND | MAX1827ETL |
| 2156-MAX1827ETL±ND | MAX1827ETL+ |
| 2156-MAX6848KATD3-ND | MAX6848KATD3 |
| 505-MAX6775LTB+TTR-ND,2156-MAX6775LTB+T-ND | MAX6775LTB+T |
| 2156-MAX8568BETE-ND | MAX8568BETE |
| 2156-MAX6775LTA±ND | MAX6775LTA+ |
| 2156-MAX6442KAEISD3-T-ND | MAX6442KAEISD3-T |
| 2156-MAX6441KAEISD3-T-ND | MAX6441KAEISD3-T |
| 2156-MAX6441KAEHRD3-T-ND | MAX6441KAEHRD3-T |
| 2156-MAX6441KAKQVD3-T-ND | MAX6441KAKQVD3-T |
| 2156-DS2746G-C02+TR-ND | DS2746G-C02+TR |
| 2156-MAX1526ETM+G104-ND | MAX1526ETM+G104 |
| 2156-MAX1906XEGE-ND | MAX1906XEGE |
| 2156-MAX6428AGUR-ND | MAX6428AGUR |
| 2156-MAX6431FJUS-ND | MAX6431FJUS |
| 2156-MAX6432MRUS-ND | MAX6432MRUS |
| 2156-MAX6431MRUS-ND | MAX6431MRUS |
| 2156-MAX6432DHUS-ND | MAX6432DHUS |
| 2156-MAX6429MRUR-ND | MAX6429MRUR |
| 2156-MAX6439UTDHSD3-ND | MAX6439UTDHSD3 |
| 2156-MAX6429KTUR-ND | MAX6429KTUR |
| 2156-MAX6432EHUS-ND | MAX6432EHUS |
| 2156-MAX6441KAEISD3-ND | MAX6441KAEISD3 |
| 2156-MAX6432FJUS-ND | MAX6432FJUS |
| 2156-MAX6432ORUS-ND | MAX6432ORUS |
| 2156-MAX6430PQUS-ND | MAX6430PQUS |
| 2156-MAX6430EIUS-ND | MAX6430EIUS |
| 2156-MAX6431CIUS-ND | MAX6431CIUS |
| 2156-MAX6430DHUS-ND | MAX6430DHUS |
| 2156-MAX6846KAWD3-ND | MAX6846KAWD3 |
| 2156-MAX6430EHUS-ND | MAX6430EHUS |
| 2156-MAX6431EIUS±ND | MAX6431EIUS+ |
| 2156-MAX6431EHUS-ND | MAX6431EHUS |
| 2156-MAX6429ORUR-ND | MAX6429ORUR |
| 2156-MAX6428ORUR-ND | MAX6428ORUR |
| 2156-MAX6431ORUS-ND | MAX6431ORUS |
| 2156-MAX6429DHUR-ND | MAX6429DHUR |
| 2156-MAX6427EIUR-ND | MAX6427EIUR |
| 2156-MAX6435UK-ND | MAX6435UK |
| 2156-MAX6428EHUR-ND | MAX6428EHUR |
| 2156-MAX6432EIUS-ND | MAX6432EIUS |
| 2156-MAX6431CHUS-ND | MAX6431CHUS |
| 2156-MAX6440UTFJTD7-ND | MAX6440UTFJTD7 |
| 2156-MAX6848KARD7-ND | MAX6848KARD7 |
| 2156-MAX6431EIUS-ND | MAX6431EIUS |
| 2156-MAX6429EHUR-ND | MAX6429EHUR |
| 2156-MAX6442KAKQSD3-ND | MAX6442KAKQSD3 |
| 2156-MAX6849KAVD7-ND | MAX6849KAVD7 |
| 2156-MAX6431DHUS-ND | MAX6431DHUS |
| 2156-MAX6441KAKQVD3-ND | MAX6441KAKQVD3 |
| 2156-MAX6437UT-ND | MAX6437UT |
| 2156-MAX6439UTEISD3-ND | MAX6439UTEISD3 |
| 2156-MAX6849KASD3-ND | MAX6849KASD3 |
| 2156-MAX1526ETM-ND | MAX1526ETM |
| 2156-MAX8695PELR+T-ND | MAX8695PELR+T |
| 2156-MAX1612EEE±ND | MAX1612EEE+ |
| 2156-MAX1666AEEP±ND | MAX1666AEEP+ |
| 2156-MAX1773AEUP-ND | MAX1773AEUP |
| 2156-MAX1773EUP±ND | MAX1773EUP+ |
| 2156-MAX17050X-C01+T10-ND | MAX17050X-C01+T10 |
| 2156-MAX1894XEEE-ND | MAX1894XEEE |
| 175-MAX17047G+T10TR-ND,175-MAX17047G+T10CT-ND | MAX17047G+T10 |
| 505-MAX17320X20±ND | MAX17320X20+ |
| 2156-DS2437S/TR/-ND | DS2437S/T&R/ |
| 2156-MAX17077ETM±ND | MAX17077ETM+ |
| MAX6780LTB+TTR-ND,MAX6780LTB+TCT-ND,MAX6780LTB+TDKR-ND,2156-MAX6780LTB+T-ND | MAX6780LTB+T |
| 2156-MAX1613EEE±ND | MAX1613EEE+ |
| 2156-MAX8697SEWQ+T-ND | MAX8697SEWQ+T |
| 2156-MAX1781ETM+C6D-ND | MAX1781ETM+C6D |
| 2156-MAX1789EUI+T-ND | MAX1789EUI+T |
| 2156-MAX1789EUI+CBH-ND | MAX1789EUI+CBH |
| 2156-MAX6430ORUS-ND | MAX6430ORUS |
| 2156-DS1610-ND | DS1610 |
| 2156-MAX1787EUI+GH8-ND | MAX1787EUI+GH8 |
| MAX17049G±ND | MAX17049G+ |
| MAX38888ATD±ND | MAX38888ATD+ |
| MAX17301X±ND | MAX17301X+ |
| 505-MAX17300X±ND | MAX17300X+ |
| 2156-MAX6777LT±ND | MAX6777LT+ |
| 2156-MAX4919BETD±ND | MAX4919BETD+ |
| 2156-MAX6780LTB±ND | MAX6780LTB+ |
| 2156-MAX6427EIUR±ND | MAX6427EIUR+ |
| 2156-MAX6427DHUR±ND | MAX6427DHUR+ |
| 2156-MAX6778LT±ND | MAX6778LT+ |
| 2156-MAX6775LTB±ND | MAX6775LTB+ |
| 2156-MAX6437UT±ND | MAX6437UT+ |
| 175-MAX77972EWX±ND | MAX77972EWX+ |
| DS2784G±ND | DS2784G+ |
| DS2775G±ND | DS2775G+ |
| 2156-MAX1666VEEP±ND | MAX1666VEEP+ |
| 505-MAX38886ATD±ND | MAX38886ATD+ |
| MAX17303X±ND | MAX17303X+ |
| 175-MAX17320G20+TTR-ND,175-MAX17320G20+TCT-ND,175-MAX17320G20+TDKR-ND | MAX17320G20+T |
| 175-MAX17335X22+TTR-ND,175-MAX17335X22+TCT-ND,175-MAX17335X22+TDKR-ND | MAX17335X22+T |
| MAX14607EWL+TTR-ND,MAX14607EWL+TCT-ND,MAX14607EWL+TDKR-ND | MAX14607EWL+T |
| MAX17211G±ND | MAX17211G+ |
| MAX6430EGUS+TTR-ND,MAX6430EGUS+TCT-ND,MAX6430EGUS+TDKR-ND | MAX6430EGUS+T |
| MAX8682ETM±ND | MAX8682ETM+ |
| 175-MAX17332X22+TTR-ND,175-MAX17332X22+TCT-ND,175-MAX17332X22+TDKR-ND | MAX17332X22+T |
| MAX17048G±ND | MAX17048G+ |
| MAX14671EWL+T-ND | MAX14671EWL+T |
| MAX16914AUB+T-ND | MAX16914AUB+T |
| MAX16915AUB+T-ND | MAX16915AUB+T |
| DS2703U+T&R-ND | DS2703U+T&R |
| 505-MAX6778LT+TTR-ND | MAX6778LT+T |
| 505-MAX17313X+TTR-ND | MAX17313X+T |
| 505-MAX17303G+TTR-ND | MAX17303G+T |
| 505-MAX17313G+TTR-ND | MAX17313G+T |
| 505-MAX17313G±ND | MAX17313G+ |
| MAX17201X+T0E-ND | MAX17201X+T0E |
| MAX17211X+T-ND | MAX17211X+T |
| MAX17211X+T0E-ND | MAX17211X+T0E |
| MAX17211G+T-ND | MAX17211G+T |
| MAX17201G+T0E-ND | MAX17201G+T0E |
| MAX17211G+T0E-ND | MAX17211G+T0E |
| 505-MAX6427EIUR+TTR-ND | MAX6427EIUR+T |
| 505-MAX17320X10+TTR-ND | MAX17320X10+T |
| 505-MAX6780LTA+TTR-ND | MAX6780LTA+T |
| 505-MAX6779LTB+TTR-ND | MAX6779LTB+T |
| 505-DS2703U±ND | DS2703U+ |
| MAX16916GUB/V+T-ND | MAX16916GUB/V+T |
| 505-MAX17320X22+TTR-ND | MAX17320X22+T |
| 505-MAX17320G10+TTR-ND | MAX17320G10+T |
| 505-MAX17320X12+TTR-ND | MAX17320X12+T |
| MAX17205X+T-ND | MAX17205X+T |
| MAX17205X+T0E-ND | MAX17205X+T0E |
| MAX17215X+T-ND | MAX17215X+T |
| MAX17215X+T0E-ND | MAX17215X+T0E |
| 505-MAX17300G+TTR-ND | MAX17300G+T |
| 505-MAX17310G+TTR-ND | MAX17310G+T |
| 505-MAX6427ORUR+TTR-ND | MAX6427ORUR+T |
| MAX17205G+T0E-ND | MAX17205G+T0E |
| MAX17215G+T0E-ND | MAX17215G+T0E |
| 505-MAX17302X+TTR-ND | MAX17302X+T |
| 505-MAX17312X+TTR-ND | MAX17312X+T |
| 505-MAX17312G+TTR-ND | MAX17312G+T |
| 505-MAX17302G+TTR-ND | MAX17302G+T |
| MAX14654EWC+T-ND | MAX14654EWC+T |
| MAX14655EWC+T-ND | MAX14655EWC+T |
| 505-MAX17320G22+TTR-ND | MAX17320G22+T |
| 505-MAX17320G12+TTR-ND | MAX17320G12+T |
| 505-MAX17302G±ND | MAX17302G+ |
| 505-MAX17312G±ND | MAX17312G+ |
| 505-MAX17301G+TTR-ND | MAX17301G+T |
| 505-MAX17311G+TTR-ND | MAX17311G+T |
| 505-MAX17311X+TTR-ND | MAX17311X+T |
| 505-MAX17300X+TTR-ND | MAX17300X+T |
| 505-MAX17310X+TTR-ND | MAX17310X+T |
| 505-MAX17311G±ND | MAX17311G+ |
| MAX17040G+TTR-ND,MAX17040G+TCT-ND,MAX17040G+TDKR-ND | MAX17040G+T |
| DS2746G+T&R-ND | DS2746G+T&R |
| MAX8672ETD+T-ND | MAX8672ETD+T |
| DS2786BG+T&R-ND | DS2786BG+T&R |
| 505-MAX17205X±ND | MAX17205X+ |
| 175-MAX17049G+T10TR-ND,175-MAX17049G+T10CT-ND,175-MAX17049G+T10DKR-ND | MAX17049G+T10 |
| 505-MAX20095ATIA/VY+TTR-ND | MAX20095ATIA/VY+T |
| DS2780G+T&R-ND | DS2780G+T&R |
| DS2764AE+T&R-ND | DS2764AE+T&R |
| MAX6776LTA+TTR-ND,MAX6776LTA+TCT-ND,MAX6776LTA+TDKR-ND | MAX6776LTA+T |
| 505-ADES1756GCB/V+TTR-ND | ADES1756GCB/V+T |
| MAX20335BEWX+T-ND | MAX20335BEWX+T |
| DS2780E+T&R-ND | DS2780E+T&R |
| DS2777G+T&R-ND | DS2777G+T&R |
| DS2776G+T&R-ND | DS2776G+T&R |
| DS2778G+T&R-ND | DS2778G+T&R |
| DS2775G+T&R-ND | DS2775G+T&R |
| DS2764BE+T&R-ND | DS2764BE+T&R |
| 505-ADES1755GCB/V+TTR-ND | ADES1755GCB/V+T |
| 505-ADES1754GCB/V+TTR-ND | ADES1754GCB/V+T |
| MAX17841BGUE+T-ND | MAX17841BGUE+T |
| DS2762BE+T&R-ND | DS2762BE+T&R |
| DS2784G+T&R-ND | DS2784G+T&R |
| MAX20303CEWN+T-ND | MAX20303CEWN+T |
| MAX20303DEWN+T-ND | MAX20303DEWN+T |
| MAX20303HEWN+T-ND | MAX20303HEWN+T |
| MAX20303AEWN+T-ND | MAX20303AEWN+T |
| MAX20303EEWN+T-ND | MAX20303EEWN+T |
| MAX20303GEWN+T-ND | MAX20303GEWN+T |
| 505-MAX20303LEWN+TTR-ND | MAX20303LEWN+T |
| 505-MAX20303JEWN+TTR-ND | MAX20303JEWN+T |
| MAX1259CWE+T-ND | MAX1259CWE+T |
| 505-MAX17852ACB/V+TTR-ND | MAX17852ACB/V+T |
| MAX17830GUN+T-ND | MAX17830GUN+T |
| MAX17843ACB/V+T-ND | MAX17843ACB/V+T |
| MAX6431NQUS+T-ND | MAX6431NQUS+T |
| MAX6428BGUR+T-ND | MAX6428BGUR+T |
| MAX11080GUU±ND | MAX11080GUU+ |
| MAX11068GUU±ND | MAX11068GUU+ |
| MAX11068GUU+T-ND | MAX11068GUU+T |
| MAX11080GUU+T-ND | MAX11080GUU+T |
| DS2731E±ND | DS2731E+ |
| DS2731E+T&R-ND | DS2731E+T&R |
| DS2703G+T&R-ND | DS2703G+T&R |
| MAX8682ETM+T-ND | MAX8682ETM+T |
| MAX17041G+T-ND | MAX17041G+T |
| 175-MAX17043G+TTR-ND,175-MAX17043G+TCT-ND,175-MAX17043G+TDKR-ND | MAX17043G+T |
| MAX11080GUU/V±ND | MAX11080GUU/V+ |
| MAX11080GUU/V+T-ND | MAX11080GUU/V+T |
| MAX17044G+T-ND | MAX17044G+T |
| MAX11081GUU/V+T-ND | MAX11081GUU/V+T |
| MAX17040G+U-ND | MAX17040G+U |
| MAX17043G+U-ND | MAX17043G+U |
| MAX17040X+U-ND | MAX17040X+U |
| MAX17048X±ND | MAX17048X+ |
| MAX17049X±ND | MAX17049X+ |
| MAX11068GUU/V+T-ND | MAX11068GUU/V+T |
| MAX17043X±ND | MAX17043X+ |
| MAX17040X+T10-ND | MAX17040X+T10 |
| MAX17043X+T10-ND | MAX17043X+T10 |
| MAX17044X+T10-ND | MAX17044X+T10 |
| MAX17049X+T10-ND | MAX17049X+T10 |
| MAX16916GUB/V±ND | MAX16916GUB/V+ |
| MAX1924VEEE±ND | MAX1924VEEE+ |
| MAX17055EWL±ND | MAX17055EWL+ |
| MAX17840AGUN/V+T-ND | MAX17840AGUN/V+T |
| MAX20303BEWN±ND | MAX20303BEWN+ |
| MAX17260SEWL±ND | MAX17260SEWL+ |
| MAX17262REWL±ND | MAX17262REWL+ |
| MAX6433UK/GG8-ND | MAX6433UK/GG8 |
| MAX6776XKA±ND | MAX6776XKA+ |
| MAX17302X±ND | MAX17302X+ |
| MAX17311X±ND | MAX17311X+ |
| MAX17312X±ND | MAX17312X+ |
| MAX17313X±ND | MAX17313X+ |
| 505-MAX17853ACB/V+TTR-ND | MAX17853ACB/V+T |
| 505-MAX17041G+U-ND | MAX17041G+U |
| 505-MAX17201X±ND | MAX17201X+ |
| 505-MAX1660EEE±ND | MAX1660EEE+ |
| 505-MAX20360AEWZ±ND | MAX20360AEWZ+ |
| 175-MAX17320X22+TR-ND | MAX17320X22+ |
| MAX17260XEVKIT#-ND | MAX17260XEVKIT# |
| MAX17261GEVKIT#-ND | MAX17261GEVKIT# |
| MAX17262XEVKIT#-ND | MAX17262XEVKIT# |
| MAX17263GEVKIT#-ND | MAX17263GEVKIT# |
| 505-MAX17332X2EVKIT#-ND | MAX17332X2EVKIT# |
| 505-MAX17048EVKIT#-ND | MAX17048EVKIT# |
| MAX17303XEVKIT#-ND | MAX17303XEVKIT# |
| MAX17205GEVKIT#-ND | MAX17205GEVKIT# |
| MAX17055GEVKIT#-ND | MAX17055GEVKIT# |
| 505-MAX17320G1EVKIT#-ND | MAX17320G1EVKIT# |
| 505-MAX17330X2EVKIT#-ND | MAX17330X2EVKIT# |
| 505-MAX17320X1EVKIT#-ND | MAX17320X1EVKIT# |
| 505-MAX17300XEVKIT#-ND | MAX17300XEVKIT# |
| MAX17201GEVKIT#-ND | MAX17201GEVKIT# |
| MAX17205XEVKIT#-ND | MAX17205XEVKIT# |
| MAX17211XEVKIT#-ND | MAX17211XEVKIT# |
| MAX17215XEVKIT#-ND | MAX17215XEVKIT# |
| 505-MAX77787JEVKIT#-ND | MAX77787JEVKIT# |
| 505-MAX77789EVKIT#-ND | MAX77789EVKIT# |
| 505-MAX17320G2EVKIT#-ND | MAX17320G2EVKIT# |
| MAX17301XEVKIT#-ND | MAX17301XEVKIT# |
| MAX17211GEVKIT#-ND | MAX17211GEVKIT# |
| MAX17215GEVKIT#-ND | MAX17215GEVKIT# |
| MAX17055XEVKIT#-ND | MAX17055XEVKIT# |
| 505-MAX17260GEVKIT#-ND | MAX17260GEVKIT# |
| 505-MAX77751CEVKIT#-ND | MAX77751CEVKIT# |
| 505-MAX20342EVKIT#-ND | MAX20342EVKIT# |
| MAX17311XEVKIT#-ND | MAX17311XEVKIT# |
| 505-DS2788EVKIT±ND | DS2788EVKIT+ |
| 505-MAX17049EVKIT#-ND | MAX17049EVKIT# |
| MAX17313XEVKIT#-ND | MAX17313XEVKIT# |
| 175-MAX17300GEVKIT#-ND | MAX17300GEVKIT# |
| MAX17261XEVKIT#-ND | MAX17261XEVKIT# |
| MAX17201XEVKIT#-ND | MAX17201XEVKIT# |
| 175-MAX17335X2EVKIT#-ND | MAX17335X2EVKIT# |
| 505-MAX77963EVKIT#-ND | MAX77963EVKIT# |
| 505-MAX17049XEVKIT#-ND | MAX17049XEVKIT# |
| 505-MAX17058EVKIT#-ND | MAX17058EVKIT# |
| 505-MAX17048XEVKIT#-ND | MAX17048XEVKIT# |
| MAX17302XEVKIT#-ND | MAX17302XEVKIT# |
| MAX17312XEVKIT#-ND | MAX17312XEVKIT# |
| 505-MAX17310XEVKIT#-ND | MAX17310XEVKIT# |
| 505-MAX17047EVKIT#-ND | MAX17047EVKIT# |
| 505-DS2782EVKIT±ND | DS2782EVKIT+ |
| 505-DS2786EVKIT±ND | DS2786EVKIT+ |
| MAX17050EVKIT#-ND | MAX17050EVKIT# |