SIT9102AI-243N25E200.00000 is this part which showing in the DigiKey website is with centre pad

SIT9102AI-243N25E200.00000 , this part which is showing website is with the centre pad
since the customer need with the centre pad

Greetings,

According to the portions of the datasheet highlighted below, the 2nd digit after the dash in the part number specifies the package type. The “4” in that position specifies a 7x5mm package with center pad.