Hi,
I was looking at your 2064-K-TS-001-ND touch screen. Does that come with a linux driver? If not, do you have any touch screens that have linux drivers?
Thanks,
Chris
This TS050 Touchscreen is designed to work with Khadas Products:
- Edge2
- VIM4
- VIM3/3L
- Edge-V
- Captain Carrier Board
It uses the FT5336 chipset, which is mainline. Making sure you're not a bot!
Regards,
Hi Robert,
Thanks for replying. I hope you had a nice weekend. Thanks for providing the links. I did not see the FT5336 in the code you referenced, but I will assume the driver will mostly support the functionality.
Best Regards,
Chris
Dug into Khada’s git tree… common_drivers/arch/arm64/boot/dts/amlogic/kvim4.dts at khadas-vims-5.15.y · khadas/common_drivers · GitHub
ft5336:ft5336@38 {
compatible = "edt,edt-ft5336", "ft5x06";
reg = <0x38>;
interrupt_pin = <&gpio GPIOM_8 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpio GPIOM_9 GPIO_ACTIVE_HIGH>;
status = "okay";
};
They have not touched the mainline input driver: History for drivers/input/touchscreen/edt-ft5x06.c - khadas/linux · GitHub
Regards,
Hi Robert,
I failed to mention I am hoping to use 64 bit linux “amd64.” I believe this is a separate and distinct architecture from ARM64. I can keep looking. Thanks for all your efforts.
Best Regards,
Chris
Well, amd64 doesn’t use device-tree’s, and that display was designed for Khada products. So without knowing more about your hardware design, that display would probally be a bad choice.
For an off the shelf amd64 system, you’d be best looking HDMI screen with a USB based touchscreen adapter..
Something like: https://www.digikey.com/en/products/detail/dfrobot/DFR1170/26460582 ( 10.5” IPS 1920x1280 FHD 100% sRGB Portable USB-C and HDMI Display for Raspberry Pi They don’t list the ‘usb’ driver, probably native usb-mouse)
Regards,
Hi Robert, The hardware design is very much fluid right now. There is nothing to know except we are hoping to use Linux for the software. I will look into what you suggested. Thanks for providing that link for the DF Robot. I am going to check it out. We really like DigiKey.
Biggest thing you should figure out, is the display output, whether it’s lvds, eDP, HDMI etc.. That’ll get you into a panel, then what touchscreen drivers are available..
Regards,