Trying to find motor connector for Roomba


I am trying to find this connect - it is used in a Roomba, the motor plugs into it. The width is 6.30mm and length is 11.85mm. There are 6 pins.

Thanks,
Ian McTavish

Hello and welcome to the TechForum. Trying to ID a connector is difficult because the dimensions are not searchable on the website you have to check the datasheet for that information. The pitch of the connector can help that is the distance from the center of one contact to the center of the next one. The biggest issue is the fact that manufacturers connectors do not work with each other you will have to measure the distance of the opening and then hunt datasheet by datasheet. The connector can also be application specific to the Roomba manufacturer. This is an issue we receive requests on many times.
Link to parts we have in stock - https://www.digikey.com/short/rhv44h7h