Typo in Abracon AANI-CH-0029 datasheet

------Question for AANI-CH-0029 Please Put your question below------

The spec sheet for Abracon AANI-CH-0029 (535-AANI-CH-0029TR-ND) appears to have a typo: it says:

Nominal Inductance: 7 uH

The stamping on the part says 4R7, indicating a 4.7uH inductance. I confirmed with an LCR meter that this is indeed the case. Also, I tested the coil with an ST25DV04KC-IE6C3 and it worked just fine (reading distance is small, but good enough for our purposes).

Abracon might sell a lot more of this coil once the typo is fixed.

Hello,
Welcome to the DigiKey TechForum. I have a sent a request to the manufacturer for information on this value and will post what I receive from them.

Great - thanks for following up!

Yes - the datasheet information is incorrect. The actual value is supposed to be 4.7 nH.

Abracon will raise an ECN and update the datasheet accordingly.

Thank you so much for highlighting this to us.

Steve,

That’s progress. I sure hope “nH” is a typo, though. It’s 4.7 μH for sure.

Sorry, yes it is.

Oh, good. Thanks for confirming!