Having trouble identifying this inductor. Diameter 7.79 mm, Lead spacing 4.42mm, height 8.34mm. is it 2200 uH?
Hello,
Using a quick search for any and all ‘222 inductor’ images online, I found that the corresponding datasheets point to a marking pattern of two significant digits plus the ‘number of zeros’ in uH. So, you are probably correct to assume 2200uH or 2.2mH depending on how a site lists this value. I made a short list of relevant products from our “Fixed Inductors” category: [ 2200uF (2.2mH) Radial Lead ].
Hi,
I have an Inductor that I am finding really hard to source online. Mainly because
a) The markings on the component are very faded and difficult to make out
b) I have no idea what the markings mean, so don’t know what replacement part to look for
I can make out:
first line: 0098k (could be D098K or C098k) - the first character is a bit feint
second line: 99239 - this is clearer, so I am confident of the numbers
It is about 6mm wide and 9mm tall without the pins
Any help you could provide would be greatly appreciated!
Many thanks in advance.
Looking at your number I wondering if that maybe 393K , looking at RL895-393K it could be 393k please check otherwise what you give does not match standard values.