Würth
Webinar Date: April 16, 2026
Key Takeaways
- Optimize PCB space and reduce total BOM cost with compact LAN transformer solutions.
- Improve insulation strength and meet demanding surge requirements.
- Enhance signal integrity through superior symmetry and low insertion loss.
- Select the right LAN component based on application needs, protection level, and performance goals.
Frequently Asked Questions
I have very limited PCB space but need 1000 Mbit Ethernet. What’s your best recommendation?
- The presentation highlights 100 Mbit integrated RJ45 modules, but similar integrated solutions are also available for 1 Gbit and even 10 Gbit Ethernet. For a 1 Gbit application, it’s recommended to use a matching 1 Gbit integrated RJ45 module to optimize performance while saving space in the design.
What is the purpose of a common mode choke in an Ethernet LAN design?
- Differential mode refers to currents in opposite directions that create magnetic fields in a core which ideally cancel each other, minimizing inductive effects. If this cancellation is not perfect, some net magnetic flux appears, introducing inductance that can influence (often attenuate) noise. This helps prevent noise from propagating, particularly toward components like a common mode choke, and is used to reduce noise between different lines.
How do I know whether my PHY chip is current-mode or voltage-mode, and does it really matter for my component selection?
-
It can be difficult to find in the PHY chip datasheet, but application notes and design recommendations explain the key difference between current-mode and voltage-mode designs. In current-mode setups, the middle pin of each channel must be connected to Vcc. In voltage-mode designs, Vcc is already integrated in the PHY, so no external connection is needed.
-
Problems can arise if you mistakenly follow RJ45 connector recommendations meant for current-mode (e.g., connecting Vcc to all middle pins) while using a voltage-mode design. This mismatch can cause issues during prototyping or lab testing, making it an important detail to verify early.
What happens to the common-mode choke performance when I run PoE current through it? Do I need to worry about core saturation?
- Components designed for PoE applications differ from non-PoE parts by using larger cores and thicker wires to handle higher currents without core saturation or damage. Because space is limited in integrated connector modules (ICMs), their current capacity is lower, while the highest current handling is typically found in discrete LAN magnetics modules (e.g., LAN AQ or similar discrete designs).
Does Wurth have any Ethernet-compatible jacks that are smaller than RJ45 connectors for embedded projects with limited space?
- For Ethernet designs, a single-port connector can reduce size compared to larger multi-port options. Standard RJ45-based solutions can also vary significantly in size: integrated connector modules (ICMs) are typically the most compact fully integrated option, but even RJ45 connectors come in smaller variants - such as vertical (up- or down-facing) layouts and unfiltered versions - that can further save space depending on the design.
Why do some magicJacks have the common mode choke on the PCB side instead of the RJ45/cable side?
- The key point is that handling noise, especially with common mode chokes, depends on identifying the source. When testing in an EMC lab, you need to determine where the noise originates. If your application is generating noise, the choke should be placed on the source (the “fire”) side. If the noise is entering from outside and causing issues, it should be addressed on the cable side.
Can you please describe grounding techniques and reasons. What “ground” to use for the RJ45 case? Should discrete magnetics be referenced above a copper pour? What net? I’ve seen a lot of contradictory and vague advice.
- You have two options. Option 1: Continuous System Ground Plane (good from EMC perspective) and Option 2: Split Ground Plane (Chassis + System), In chapter 4.5 of this application guide you can find more information and test data.
Can you explain what are the applications when we need the EMI fingers on RJ45? Will they act as an antenna?
- Although an RJ45 connector with EMI fingers may look like it has “floating” metal parts (like an antenna), that’s not how it functions in a real system. In an actual application, the EMI fingers make contact with the metal enclosure, while also connecting to the PCB ground. This ensures they are properly grounded on both sides, preventing them from acting as antennas and instead helping with shielding and EMI control.
Is WE-STST also 100% automated production like LAN AQ?
- Yes, it is a fully automated product. Inside of the LAN AQ, you can find some of the STST parts inside.
Can you explain Cat5e and Cat3 Ethernet Modules? When to use? I have noticed that Cat5e pin sequence is not in order like standard, is there a reason?
- The category defines the maximum datarate (based on the maximum frequency). The pin sequence depends on the used connector. General used pairs for Ethernet over RJ45: J1 - J2, J3 - J6; J4 - J5, J7 - J8.
Does the metal top on WE-LAN AQ act as shielding?
- Intended yes, but as it is not connected → floating metal, therefore no shielding effect.
Is the “ICM” series rated for -40 to +85 deg C?
- Most of the “ICM” series is rated for this temperature, due to industrial applications.
Does WE have any ICMs for Single-Pair Ethernet, automotive or industrial?
- It was attempted to develop an integrated module for Single-Pair Ethernet but didn’t bring it to market because the connector size was too large, making the space savings inadequate.
Product Solutions from Würth
Here are some solutions we have to offer from Würth surrounding this topic.
LAN AQ Solutions
ICM RJ45 Connectors
WE-STST Series Transformers
Referral Webinar Link
If you would like more information from this webinar, please review the details below.