What are the part numbers for the parts in this video?

I’m trying to find the part numbers for the connectors in the following video:

Please help!

The second connector in the video is similar to the following:

35312-1460

and mates with the following:

35155-1400

Hello,
Welcome to the DigiKey TechForum. Closest option I found for the 5 position connector is DigiKey part WM3145-ND. This connector is very similar to the dimensions you have listed in the video. The 14 position connectors you listed are obsolete but we do have part WM26757-ND and the mate to this part WM13238-ND which may work for you. Contacts are sold separate and can be found on the links I provided, you will need to scroll down on the pages and view the associated product.

1 Like

Thank you so much for the feedback on the first connector! I will purchase a sample and test it out.

I also think that I’ve found the series number for the second connector. Upon further inspection, this one actually had text on its side (god, if only more of them had this). After looking it up, I found it:

35184-1000

Thank you for your help!