My initial question….“I am student at the University of North Dakota doing a senior design project. We are making an Active noise cancelling system. We plan to have a frequency range of 50-500 Hz (1000 Hz if we can get there). We are looking at the EVAL-ADAU1466Z board but unsure if this is the best option. We are in testing mode now but need options quickly. Will this board work or can you offer suggestions to alternative options? Lead time is also VERY important. We need something that can be delivered in 7 days or less once a decision is made. We would like a board(controller) that is plug in ready so all we have to do is add our FxLMS algorithm and let it run. We do not plan to develop our own PCB board. Here is the board that was suggested but alternative would be nice also. EVAL-ADAU1466Z
This was the response…”Thank you for contacting DigiKey , we only have two options that will be plug and play for eval kits that are in stock and can ship today , they are part numbers 505-EVAL-ADAU1467Z-ND and 505-EVAL-ADAU1466Z-ND , I am not sure if these will do what you are looking for I would suggest going through the data sheets and links in them to see if these will be the best options for what you are looking to do , there are software downloads documents and ap notes listed on the data sheets for you to look at on page 1 of each below.”
https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADAU1466Z_UG-1135.pdf
https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADAU1467Z-UG-1134.pdf
then my final response (the part i need an answer to)…”Thank you for the recommendations. I only have one other question. Since we are trying to do high sample rates for freq 50-500 HZ (or even 1000 Hz if we can) it is probably not a good idea to also use the recommendations for charting, controls, etc. In your option, would I be able to use one of these suggestions as a slave board and have a master board that is used for Wi-Fi, Bluetooth, IoT, etc? Or would it not interface very well? Ideally, wanting to use Arduino IDE platform if possible then planning to use Blynk system as the system controls app.”