Which basic switches are resistant to vibration and impact?

Question:

Which basic switches are resistant to vibration and impact?

Block

Answer:

The larger the OF (operating force) standard value in the state of the button being pushed, the more resistant it will be against vibration and impact. Therefore, it is recommended to select the basic switch with the largest OF among available sizes and electrical ratings.

Block

Explanation:

Since the contact pressure of a basic switch with high OF is high, it is advantageous against vibration and impact when the switch is in the free state (FP) (when used under the same conditions). However, vibration and impact are greatly affected by the direction of the applied force. Please evaluate the vibration and impact resistance by attaching it to the actual equipment before deciding whether to use the switch.

Block

Product category

Switches Basic Switches


Classification

Trouble shootings


Related keywords

Basic Switch
Vibration Impact
Operation Force

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20045