I followed the instructions here
and I have successfully booted into my freshly installed system. I also installed xfce which I successfully can start the DE by issuing startx. One thing though.
When I enter xrandr from within xfce I get the following
xrandr: Failed to get size of gamma for output default
Screen 0: minimum 1280 x 1024, current 1280 x 1024, maximum 1280 x 1024
default connected 1280x1024+0+0 0mm x 0mm
1280x1024 0.00*` `
Accordingly there is no HDMI-0 output, so I can not issue
xrandr --output HDMI-0 --mode 1024x768 --rate 60
Is it something wrong with my configuration?
Furthermore, do I need to run the sgx_build_modules.sh script?
@umbaman thanks for the report, just confirmed, that xrandr no longers shows “HDMI-0”…
ubuntu@arm:~$ xrandr -q
xrandr: Failed to get size of gamma for output default
Screen 0: minimum 1280 x 1024, current 1280 x 1024, maximum 1280 x 1024
default connected 1280x1024+0+0 0mm x 0mm
1280x1024 0.00*
ubuntu@arm:~$ xrandr --listmonitors
xrandr: Failed to get size of gamma for output default
Monitors: 1
0: +default 1280/339x1024/271+0+0 default
ubuntu@arm:~$ xrandr --listproviders
Providers: number : 0
Regards,
@RobertCNelson Thanks for the reply.
Could you please elaborate on the process of building and incuding sgx modules.
I can see the sgx_build_modules.sh script. I guess it needs to be run
Running only the create package isn’t enough, because the corresponding modules are not installed on the target machine.
So is there a step I am missing?
Kind Regards
@umbaman, first you need to be aware, that we only have “sgx” working with the bone kernels, in “FBDEV” mode, aka no mouse cursor/xorg/etc… It’s been forward ported since the 3.8.x days, so there will be bugs…
There’s two scripts in the repo
sgx_build_modules.sh and sgx_create_package.sh
They are really the same script, “sgx_create_package.sh” assumes you’ve installed the sgx modules from the apt repo for your kernel. Where as the “sgx_build_modules.sh” builds both the modules and the create package install script.
Regards,