15038PB-B3L-CP-U0-ND protection rating

Hi, What is the protection rating for the fan 15038PB-B3L-CP-U0-ND

Also is the fan meant for wet location?

Hello purchasing37,

Welcome to the DigiKey TechForum.

The manufacture’s website lists 2 fans with this number, as a 50Hz & 60Hz version.

Here is the link to the 60Hz version:

15038PB-B3L-CP-U0_60Hz | NMB Technologies

Both the 50Hz & 60Hz fans have an ingress protection of IP69K, so they should be able to operate in wet conditions.