BSB03505HP-00 Customize meet IP67 Standard

------Question for BSB03505HP-00 Please Put your question below------

Currently, we are using the BSB03505HP-00 for our design, and I would like the BSB03505HP-00 to meet the IP67 standard.
Can you customize the BSB03505HP-00 to achieve IP67 compliance?

And I saw BSB03505HP-00 have range temperature is 0°C to 60°C . I want the fan to operate in the range of -20°C to 60°C. Is that possible?

Thank you and best regards

Hello,
Welcome to the DigiKey TechForum. You will need to contact Delta directly to see if they will customize a fan for you.