2A471J Mylar Polyester Film Capacitor




Need help please they are for a denon avr-x4500h on the 4 channel and 5 channel amp board. I was trying to set the idling current and my probes slipped and shorted out almost all the caps plus other stuff.
Plus i need a 2w.47 flame proof resistor


Plus a few of the black im guessing transistors they both are with the picture with the resistor.

ns2_1982

Aluminum capacitors 470 and 10uF from the link below you will have to apply filters for the size of these caps to narrow down the search .

Film capacitors , you will need to check the size to see if any of these will work for you .

.47 ohm 2W flame proof resistor , we do not have any to offer

KIA1024-Y-AT , cannot confirm part number
KTC3206Y-AT , No replacement to offer

Thanks Craig

For the resistor can use a resistor that is very close or would that mess up my amp. Im new to all of this.

Yahoo Mail: Search, Organize, Conquer

Hello @ns2_1982,

This looks like a viable solution. Yes, you will need to bend to fit.

BTW, be sure to check out HiFi Engine, they may have the schematic for you receiver or a closely related model.

Welcome to the community and watch those probes - we’ve all been there!

Best Wishes,

APDahlen

P.S. The other parts may be transistors specifically 2SA1024 and 2SC3206.

The flame proof resistor that i need is 2w 0.47ohm do yall have 0.48

Hello ns2_1982,

The resistor that APDahlen had recommended above would be a 0.47Ohm (the same as 470mOhm), 2W, flame proof resistor.