PHLITSCH PART NUMBER 96226.6
WHAT ARE THE DIMENTIONS OF
THE HOLES IN THE GROMMET?
PHLITSCH PART NUMBER 96226.6
WHAT ARE THE DIMENTIONS OF
THE HOLES IN THE GROMMET?
This looks to have 4x holes that are 6.5mm diameter each.
Note: Conta-Clip is apart of PFLITSCH
96226.6.pdf (73.4 KB)
WOULD YOU KNOW THE PART number for
M32 2 hole X 13
How many holes would you be wanting that to have at the 13mm size?
I need 2 holes OD OF MY CABLE IS 0.465”
I see the 2x holes now.
Cable and Cord Grips | Cables, Wires - Management | DigiKey
For 0.465"
That would be ~ 11.811mm
There is an option that would be closer at 12mm.
96257 type.
Cable and Cord Grips | Cables, Wires - Management | DigiKey
WHAT ABOUT 23255?
Nothing comes up on 96257
The link I gave shows those items we have on our site.
A search for “96257” would also need a modifier of “cable gland” to get just those items to show upon the site.
“23255” or (as I had found) “23255.9” is a sealing plug that can be used to fill the unused blanks in the cable glands like the 96226.6.
This would be for an 11mm hole.
Or are you referring to the items in the below link?
Cable and Cord Grips | Cables, Wires - Management | DigiKey
For those cable glands from what I can tell they would not come with inserts.
An insert would need to be ordered separately.
The below link shows the items I had found that look to be the correct size for that 23255 glands.
UFE 55 Pflitsch | Bushings, Grommets