Hello, I’m looking for a replacement transformer. The failed one I’m replacing is this:
Pacific Electronics Corporation
MODEL:A71825DC
AC ADAPTER
CLASS 2 TRANSFORMER INPUT: 120VAC 60Hz 50W OUTPUT:17VAC 2350mA
Please let me know if you carry a transformer that would be a suitable replacement.
Thanks
Hi dfinley8082,
The BPE2F is the nearest product that we stock. It is rated for 16Vac at 2.5A. The typical behavior of such transformers is that the voltage will tend to be slightly higher as the current draw decreases, so at 2.35A, it would likely be very close to your 17Vac specification.

1 Like
Thanks, I’ll order that one.
Dave
1 Like