Access to "ICECUBE 2012.03" for programming ICE65 FPGA Family?

Hi,

We are in need of the Silicon-Blue/Lattice-Semiconductor “ICECUBE 2012.03” IDE software in order for us to be able to program FPGA chips from the ICE65 family. Please let us know if anyone can help us with this. Thanks.

Hany

Hi @hanyabushall you’ll need an account with Lattice,

You can find all their archived software releases here:

https://www.latticesemi.com/Support/SoftwareArchive

Regards,

Hi @RobertCNelson thanks for the quick and helpful feedback.
Unfortunately, I have already checked this link before and the earliest version they are offering is “2012.09”. This one does not have support for ICE65 family. The one we are looking for is “2012.03”; about 2 versions earlier. I was wondering if there are some other way we can have this earlier version. Thanks.

I suppose you’ve contacted Support directly?

Looking around github, there are some open-source programmers now… Can we assume you have the final built files/hex/etc? IN which case we just need to program your device? SO, which external programmer are you using?

Or do you need to fully rebuild your project?

Regards,

Hi @RobertCNelson,

Yes, I have contacted Support directly. I have also found that a later version of Lattice Semiconductor programmer can be used to program ICE65 FPGA chips.

Unfortunately, I am in need to rebuild the project and hence having the proper programmer is not sufficient to solve the issue.

Thanks again for your help and looking forward to any other helpful suggestions.

Hi, what was the later version you found for the ice65, i have had no luck finding a version that works with the Ice65

Thanks

Hi kipper2k, Welcome to DigiKey. Our apologies for the delay. It appears from the earlier conversations that the 2012.03 is the version needed for the ice65. I will forward your request to one of our engineers to see if they have any other suggestions. Best regards, Mo

HI @kipper2k for the ice65 you need to contact Lattice directly: Lattice Support

Regards,

Thanks, they wouldnt even reply to me, however, i did find Silicon Blue ICECUBE2 sofrtware… but, unable to get a valid license file to use the synplify tool, so still stuck lol

Thanks for the reply

Brian

Hi @kipper2k Lattice was done with this product line back in 2012.

NotificationofIntenttoDiscontinuetheiCE65ProductFamily.PDF (71.8 KB)

Any stock from Rochester, is really for manufactures/oem’s still building existing designs.

Regards,

Hi, Yah. the reason i wanted thiis chip as it has 5v tolerance apparently so i wanted to test it on some old equipment. nI dis find Silicon Blue Version 2011.06 which does support the ICE65, now i just need a licence file to go with it for the Synplify tool

Brian