AD7280WBSTZ-RL

The AD7280WBSTZ-RL is coming programmed from the factory?
The SPI,alerts and etc

Greetings,

The AD7820 does not come programmed from the factory. All of the device’s configurable features and functions must be set by the user at run time.

Do I need programmer or the mcu will configure the chip when it takes power?

Configuration would be done using whatever MCU or similar device that is being used to read and process information from theAD7280.