ADBMS6830BCSWZ

We want to procure this component ADBMS6830BCSWZ
But I want to know does this component come as Preprogrammed chip?

Hello srinivas sadhu,

Welcome to the DigiKey TechForum.

This IC is programmable yes but it does not come pre-programed according to the data sheet.
ADBMS6830 (Rev. SpB) (analog.com)

Hope that helps.
Regards.

Thanks for the Input.

Does the IC responds to the commands mentioned in Datasheet.

If it does not come pre-programmed how do we program that IC.

The complete datasheet requires a signed NDA. I would think those commands would be build in to the chip. Details about programming that chip will likely require that Nondisclosure.

Mike

Aye, Gromit is correct. NDAs with Analog Devices are required to get into firmware support, per a Thread on Firmware Support on Analog Devices ADI EngineerZone forum, Here

If the commands are already build in to the chip then we no need to program that again right. It will respond to our commands.

That means the chip will come as preprogrammed.

Yes, if the commands are built in then you could just send those commands to the chip and it should respond appropriately, but, to be sure I would sign that NDA and get the details to see if it will work for you. If you call Analog and ask the same questions they may help you to some degree without the NDA.