Hi!
I’m trying to figure out the component on the picture. BN0T 18, six pin SMD. The device it’s from is an LED dimmer.
Any help is much appreciated ![]()
Thanks and all the best!
Hi!
I’m trying to figure out the component on the picture. BN0T 18, six pin SMD. The device it’s from is an LED dimmer.
Any help is much appreciated ![]()
Thanks and all the best!
Hi Janis,
I agree with Adam7, that looks to be the AOZ1282CI which we have in stock.
The marking on the data sheet page 13 shows as below snip:

Hope that helps. Have a great day.
Hey!
Thanks for the fast replies! The pin layout looks the same so it should be the right component ![]()
I’m also having trouble finding two diodes pictured below. Hope you can help with these too ![]()
Thanks alot! ![]()
Hello,
The possible part number for BBK on the first picture could be SMBJ26CA-TR on this link:
I am unable to verify the DMB
I am also not able to identify the third one. Though maybe someone else will find these .
janis, see below:
Marking DMP - it is DMP3098L
Marking 32 - t is HRF32
Marking BBK - it is SMBJ26CA-TR
32-HITACHI-HRF32.pdf (33,6 КБ)
DMB-DMP3098L.pdf (266,0 КБ)
BBK - SMBJ12CA-TR.pdf (125,9 КБ)
Good info, thanks for your contribution Adam7!
A quick follow up, it looks like we do stock the DMB3098L, linked here: DMP3098LDICT-ND (NOTE: We have the manufacturer part number listed with an additional “-7” at the end, this is notes the default packaging as a 7-inch plastic reel. It does not call out any change to specification on the part itself.)
As for the HRF32, this one is made by Hitachi and not stocked by us. Generally it’s good practice to replace a known component with the same part number, but if you have trouble sourcing the Hitachi diode, or if you just want to keep it all from the same distributor we stock an equivalent from Vishay General Semiconductor- part number SS1H9-E3/61TGICT-ND
Hope this helps!