I would like to order from DigiKey Amphenol connector receptable ER22BB11 but i am not sure what wire size support since from website descriuption and documentation is a bit unclear. My need is a connector for a 50sqmm HV wire. For the plug need of a 50sqmm wire i found the part nr but will be good to have the confirmation as well EP225011. MAny thanks for further support and replay.
Hello,
Welcome to the DigiKey TechForum. This is the 200 amp version and would have the 8mm contact size. 8mm diameter when converted to mm square will give you 50.27sqmm which will work for the wire size you need and yes, part EP225011 will work with 50sqmm.
Hi,
Many thanks for the answer. Now i would come back with one more question. On ER22BB11 can be used of 70sqmm? If not in that case should I change to ER42BB11 which support 50, 70 or 95sqmm?
I am interested also on plug EP225011 which support 50sqmm in case i would like to increase to a bigger cable 70sqmm should i order EP427011 or exist the possibility to use EP225011 and order only contact with the size of 11mm in diameter?
Thanks in advance for clarification.