オリジナルのコードでは、13番ピンを使用し、ボード上の小さなLEDが1000ミリ秒の間隔で点滅する連続ループを実現していました。このサンプルコードでは、内蔵の遅延関数を使用して、ループ関数内の各アクションの間に一時停止をかけています。この設定では、選んだピンでマイクロコントローラが機能するように、各ピンを定義する必要があります。
最初のサンプルコード
// the setup function runs once when you press reset or power the board void setup() { // initialize digital pin 13 as an output. pinMode(13, OUTPUT); }
// the loop function runs over and over again forever
void loop() {
digitalWrite(13, HIGH); // turn the LED on (HIGH is the voltage level)
delay(1000); // wait for a second
digitalWrite(13, LOW); // turn the LED off by making the voltage LOW
delay(1000); // wait for a second
}
初期コード配線図
これは、13番ピンのオンボードLEDを使用しています。以下の写真で、基板上の位置を確認できます。追加の配線は必要ありません。

拡張コード
私自身のちょっとしたプロジェクトのために、12番ピンにLEDと抵抗を追加し、13番ピンを遮断しました。そして、新しいLEDのタイミングを変えて、SOSの遭難信号をシミュレートしました。
// the setup function runs once when you press reset or power the board void setup() { // initialize digital pin 13 as an output. pinMode(12, OUTPUT); }// the loop function runs over and over again forever
void loop() {
digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level)
delay(250); // wait for quarter second
digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level)
delay(250); // wait for quarter seconddigitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(250); // wait for quarter second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(250); // wait for quarter second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(250); // wait for quarter half second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(250); // wait for quarter half second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(500); // wait for a half second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(500); // wait for half second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(500); // wait for a half second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(500); // wait for half second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(500); // wait for a half second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(500); // wait for half second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(250); // wait for quarter second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(250); // wait for quarter second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(250); // wait for quarter second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(250); // wait for quarter second digitalWrite(12, HIGH); // turn the LED on (HIGH is the voltage level) delay(250); // wait for quarter second digitalWrite(12, LOW); //turn the LED Off ( Low is the voltage level) delay(800); // wait for 800 milli seconds - when it loops without longer delay it looks like it does a different pattern
}
拡張コード配線図
赤色のワイヤは12番ピンと、ブレッドボード上の「プラス」に接続されています。
赤色のワイヤは、330Ωの抵抗器と赤色のLEDに直列に接続されています。
オレンジ色のワイヤは、ArduinoのグランドとLEDのマイナスリードに接続されています。
部品表
カートへのリンク:Digi-Key - Fast Add