この例は、アナログ入力を使用してアナログ出力を制御する方法を示しています。 この回路のポテンショメータは、LEDのパルス幅変調(PWM)を制御するために使用されます。 スケッチはまた、マッピング機能を使用して、アナログ入力範囲(0~1023)を取得し、それをアナログ出力範囲(0~255)にマッピングします。
最初のサンプルコード
//constants are used in this sketch to give names to the pins that do not change const int analogInPin = A0; const int analogOutPin = 11;//Variable set up to store the value of the potentiometer.
int sensorValue = 0;//Variable set up to store the output to the PWM (analog output)
int outputValue = 0;void setup() {
//Set up the serial communications
Serial.begin(9600);
}void loop() {
//Read the value of the potentiometer
sensorValue = analogRead(analogInPin);// map it to the range of the analog out outputValue = map(sensorValue, 0, 1023, 0, 255); //Set the PWM of the output LED to the mapped value analogWrite(analogOutPin, outputValue); // print the results to the serial monitor Serial.print("sensor = "); Serial.print(sensorValue); Serial.print("\t output = "); Serial.println(outputValue); // wait 2 milliseconds before looping back to the top delay(2);
}
初期コード配線図
拡張コード
今回の拡張コードでは、3つのLEDをPWMで制御します。そのために、アナログ入力を0~255にマッピングするのではなく、0~765、つまり3倍の幅にマッピングします。そして、マッピングされた値を使って、どのLEDが現在PWMで制御されているかを知ることができるようにします。これは、デバイスが使用している音量や電力量を示す音量計や同様のLED出力に似ています。
// Analog input pin that the potentiometer is attached to const int analogInPin = A0;// Analog output pin that the LED1 is attached to
const int analogOutPin1 = 9;// Analog output pin that the LED2 is attached to
const int analogOutPin2 = 10;// Analog output pin that the LED3 is attached to
const int analogOutPin3 = 11;//Variable set up to store the value of the potentiometer.
int sensorValue = 0;//Variable set up to store the output to the PWM (analog output)
int outputValue = 0;void setup() {
//Set up the serial communications
Serial.begin(9600);
}void loop() {
//Read the value of the potentiometer
sensorValue = analogRead(analogInPin);// map the output value to the range of the analog out(0 to 255) x 3 outputValue = map(sensorValue, 0, 1023, 0, 765); /* * In the below set of code, we take the outputValue variable and divide * it up to control 3 separate LEDs */ if (outputValue <= 255) { // if the potentiometer is in the first 3rd of travel // change LED 1 to the analog out value: analogWrite(analogOutPin1, outputValue); //make sure LED 2 and 3 are off digitalWrite(analogOutPin2, LOW); digitalWrite(analogOutPin3, LOW); } else if (outputValue >= 256 && outputValue <= 510) { // if the potentiometer is in the middle 3rd of travel // Turn on LED 1 digitalWrite(analogOutPin1, HIGH); // set LED 2 to the adjusted brightness. Subtracting 255 gets us the correct value. analogWrite(analogOutPin2, outputValue - 255); // turn LED 3 off digitalWrite(analogOutPin3, LOW); } else { // if the potentiometer is in the last 3rd of travel // Turn on LED 1 digitalWrite(analogOutPin1, HIGH); // Turn on LED 2 digitalWrite(analogOutPin2, HIGH); //We have to subtract the 510 to find the level of brightness for the 3rd LED to be set at analogWrite(analogOutPin3, outputValue - 510); } // print the results to the serial monitor Serial.print("sensor = "); Serial.print(sensorValue); Serial.print("\t output = "); Serial.println(outputValue); // wait 2 milliseconds before looping back to the top delay(2);
}
拡張コード配線図
部品表
カートへのリンク: Digi-Key - Fast Add