Question:
Are the temperature conditions for manual soldering the same as those for PCB relays?
![]()
Answer:
The temperature conditions are 350°C and within 3 seconds, or 260°C and within 10 seconds.
Although they are slightly different from those for PCB relays, perform soldering under conditions that do not give heat stress.
![]()
Explanation:
MOSFET relay manual soldering conditions
- Manual soldering must be within 3 seconds at 350°C or within 10 seconds at 260°C.
- Manual soldering conditions for VSON, S-VSON, and P-SON series products should be within 10 seconds at 260°C.
- Manual soldering can be done once. Do not reuse the product that has been removed to rework.
For more information, see Common Precautions for All MOSFET Relays
![]()
Quick tips:
Try to use a soldering iron with as low wattage as possible to reduce the effect of heat.
Please visit the link below to see this product line on the Digi-Key website
Relays | Solid State Relays | Digi-Key Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10078