Audio processing demo board

Q1 –
Customer has a request this morning for the TAS2110EVM GUI and this is still pending. I am also trying to get the TAS2110EVM working but cannot get any sound out of the module. I have connected a 5V supply to J16 and connected the USB port and have a blue LED illuminated. I have also made sure that the short links on the board are as described in table 5.1 and followed the rest of of the TAS2110EVM Users Guide. I have been waiting for the TAS2110EVM since the 4 Feb 2026 and eager to progress with the project that I am working on. I am currently running on Windows 11. Any help will be thoroughly appreciated?

Reply from TI Engineering Support;
A -

We have processed your software access request, and you should receive a confirmation email soon. Do you already have access to PurePath Console 3 and were just waiting for software link
High power class D amplifiers
Customer can click this link for downloading the software you need

In order to get audio from EVM, you first have to initialize the device, so you still need to use the GUI to be able to play audio.
While you are still in evaluation phase, you may want to check out TAS2120, which is a recent released device with new generation features compared to TAS2110

Response statement back from Customer;
Thank you for getting the TAS2110 EWM to me. I still had trouble after installing the app because I could see the clocks on J3 and J4 and even data on J5 but no sound through the speaker. Once we changed the Windows 11 control panel speaker setting from mono to 7:1 surround sound the sound then came out of the speaker
TAS2110EVM: Unable to play .wav file with STM32U5 + TAS2110EVM (Getting noise/corrupted audio) - Audio forum - Audio - TI E2E support forums