We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
CAN1 is exported to BONE_P9_26/P9_24. the CAN interface is up (listed by ifconfig). No apparent problems on BBBw. But No Rx/Tx.
From
Is device overlay needed for BBBw (4.19.50-ti-r20) ?
On bus, it is properly terminated (60 Ohm).
But, when BBBw CAN1 is connected to P9_26/P9_24, the termination becomes 83Ohm.
BBBw doesn’t have default terminator, right?
Any suggestions that something may have been neglected ?
I connected to a CAN bus. I am using PCAN for testing. I also have PCAN-Diag (PEAK). The bus itself is OK. But if connected to CAN1 on BBBw dev board, the termination from 60 Ohm to 80 Ohm. So the BBBw CAN interface has changed termination there.
&dcan1 {
status = "disabled"; /* Enable only if Profile 1 is selected */
pinctrl-names = "default";
pinctrl-0 = <&dcan1_pins_default>;
};
It says disabled. Enable only if Profile1 is selected. Don’t know what is the Profile 1. But this status is initial run-time status, right? It can be enabled through configuration without recompiling dtbo?
Also, the P9_26 seems pulled up (high). Is possible the pin mux for P9_26 has a confliction?