Hello,
I am experiencing an issue with the BPM2417SJ module where the output is 0V DC despite providing 140V-420V DC input. I have tested multiple units with the same result.
Please clarify the following for my test setup:
External Components: Are the Y-capacitors C103 and C104 (330pF) mandatory for the module to start, or can it run without them during a bench test?
Please confirm if the issue is caused by missing external Y-capacitors, incorrect parallel pin connections, or if there are mandatory feedback/sensing pins that must be jumpered for the module to activate.
Thank you very much for your support.