Any help identifying this part would be greatly appreciated. Others on the board are labled “4.7 16+”
Hello promarinesystems, welcome to the Forum!
Your capacitors appear to be tantalum caps. The one that is marked 1 and 35+ is likely a 1uf 35V capacitor like these options which are in stock. You can choose one that is the same dimensions and lead spacing as the capacitors you have. Here are the stocking options for the 4.7uf 16V capacitors.
Thank you so much!
Before you pull the old parts out, mark the positive lead locations on the PCB.
Tantalums will be damaged almost instantly from reverse polarity, some times they even explode like firecrackers.
Of course, thank you for the reminder! This community is fantastic!