Hi. I need a little help identifying these capacitors. I believe they are tantalum capacitors. One being 150uf the other is 100uf and both are three volts. Can anyone give me a viable replacement for them. They are going into an old 80s Minolta Camera. Thanks
Welcome to the forum
The search link below is in stock, radial through hole, 100uF & 150uF tantalum caps.
There are no 3V parts in stock however you can always use a higher voltage if it physically fits. So pick parts from the search based on their size.
Thanks a bunch. So a little higher voltage would be fine then? Correct?
As long as the capacitor uf value is the same.
Yes a higher voltage is OK
Hello @jaromtsmith
The parts @PaulHutch had posted would be good replacements based on the information provided, and just like PaulHutch had already said make sure to check the physical size of the original part.