My Driver is a constant current with output: 20-42v 950mA Max. The website listed it as 30w 6-12x3W. I was wondering if the 6-12x3W means anything or is that just the model number?
Anyway, my strip is a Bridgelux Gen 3 Thrive 560mm 4k. https://www.bridgelux.com/sites/default/files/resource_media/DS133%20Bridgelux%20EB%20Series%20Thrive%20Data%20Sheet%20081320%20Rev%20A.pdf
Listed drive currents of 700, 960, 1400, 1920mA, and min v is 18.5v and max 22.9.
I want to run 2 of these strips wired in series, can this driver handle this? Would the driver just reduce the current to accommodate its lower power capability?