I bought some Bridelux EB Gen 3 strips a while back, and would like to add some of their newer EB Gen3 Thrive strips to an existing setup with a Meanwell HGL-185H-48 driver. Can I do this without issue.
The strips would be the same size 560mm, and the existing strips have an typical current of .700A at 19.1v for 13.4w. The new Thrive has two listed nominal currents for the same strip 480/960ma and 350/700. For the 700ma the voltage is a little higher than the regular gen3 at 19.9.
Here are the datasheets for both strips: