Question:
Can the light convergent reflective type Optical Sensor B5W-LB detect reflective objects (mirror, glass plate) inclined at varying angles?
![]()
Answer:
In the case of detecting a glossy object, the object’s surface should be set parallel to the sensor’s sensing surface.
![]()
Explanation:
The light convergent reflective type Optical Sensor B5W-LB series has a special optical design to receive specular reflection from the sensing object. Especially when a glossy object such as a glass plate should be detected, it is necessary to consider the mounting angle of the sensor for stable detection because the receiving light intensity of the sensor significantly varies depending on the angle of the object’s glossy surface. Please refer to “Angle characteristics” (shown below) in the datasheet. According to the data, the sensor should be mounted at a right angle to the object’s surface in the vertical direction. For stable detection of glossy objects, it is recommended that the structural design and sufficient evaluation of the equipment take into account the angular variation of the sensing objects in the actual equipment.
![]()
Quick tips
This angle characteristic is the result of a measurement at the sensing distance of 30 mm. If the sensing distance can be adjusted in the equipment design, the angle characteristics can be improved by shortening the sensing distance in a range where the amount of receiving light of the sensor does not decrease, by referring to “Receiver output – sensing distance characteristics.” Use the actual equipment for consideration.
Product category
Sensors Light Convergent Reflective Sensors/Diffuse Reflective Sensors
Classification
Usage, Applications
Related keywords
Optical Sensor
Light Convergent Reflective Type Sensor
Direct Reflection
Angle Characteristics
B5W-LB
![]()
Please visit the link below to see this product line on the DigiKey website
Optical Sensors | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ