Clarification on Chamfer Position for IQD Crystal LFXTAL069404

If you have observed variation in the chamfer location (i.e., the chamfer position appears different from what is shown in the datasheet) on the IQD Frequency Crystal LFXTAL069404, as shown in the image below,
Please note that we have checked this with the manufacturer. Please see their response below:

The chamfer (the small angled corner on the crystal package) in the above photo is correct.
The real problem is that the marking printed on the top is not consistent, which is causing confusion.

The crystal will still work correctly electrically, because it only connects between pins 1 and 3. Even if the pick‑and‑place machine looks from underneath, it will still place it correctly.

The only issue happens during AOI stage. Because the marking is inconsistent, AOI machine may think the part is fitted the wrong way.

This can usually be fixed by programming the AOI machine to accept the part either way around for Xtal only.

Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
1923-830108208209TR-ND,1923-830108208209CT-ND,1923-830108208209DKR-ND 8.30108E+11
1923-830107871909TR-ND,1923-830107871909CT-ND,1923-830107871909DKR-ND 8.30108E+11
1923-830108208709TR-ND,1923-830108208709CT-ND,1923-830108208709DKR-ND 8.30108E+11
1923-LFXTAL062487TR-ND,1923-LFXTAL062487CT-ND,1923-LFXTAL062487DKR-ND LFXTAL062487
1923-830108208809TR-ND,1923-830108208809CT-ND,1923-830108208809DKR-ND 8.30108E+11
1923-830107284409TR-ND,1923-830107284409CT-ND,1923-830107284409DKR-ND 8.30107E+11
1923-830108208409TR-ND,1923-830108208409CT-ND,1923-830108208409DKR-ND 8.30108E+11
1923-830107820709TR-ND,1923-830107820709CT-ND,1923-830107820709DKR-ND 8.30108E+11
1923-LFXTAL069383TR-ND,1923-LFXTAL069383CT-ND,1923-LFXTAL069383DKR-ND LFXTAL069383
1923-LFXTAL063334TR-ND,1923-LFXTAL063334CT-ND,1923-LFXTAL063334DKR-ND LFXTAL063334
1923-LFXTAL069392TR-ND,1923-LFXTAL069392CT-ND,1923-LFXTAL069392DKR-ND LFXTAL069392
1923-LFXTAL069395TR-ND,1923-LFXTAL069395CT-ND,1923-LFXTAL069395DKR-ND LFXTAL069395
1923-830108186509TR-ND,1923-830108186509CT-ND,1923-830108186509DKR-ND 8.30108E+11
1923-830108208009TR-ND,1923-830108208009CT-ND,1923-830108208009DKR-ND 8.30108E+11
1923-830108208109TR-ND,1923-830108208109CT-ND,1923-830108208109DKR-ND 8.30108E+11
1923-LFXTAL068297TR-ND,1923-LFXTAL068297CT-ND,1923-LFXTAL068297DKR-ND LFXTAL068297
1923-LFXTAL069405TR-ND,1923-LFXTAL069405CT-ND,1923-LFXTAL069405DKR-ND LFXTAL069405
1923-LFXTAL069381TR-ND,1923-LFXTAL069381CT-ND,1923-LFXTAL069381DKR-ND LFXTAL069381
1923-LFXTAL069407TR-ND,1923-LFXTAL069407CT-ND,1923-LFXTAL069407DKR-ND LFXTAL069407
1923-LFXTAL050991TR-ND LFXTAL050991
1923-LFXTAL069387TR-ND LFXTAL069387
1923-LFXTAL069390TR-ND LFXTAL069390
1923-LFXTAL069400TR-ND LFXTAL069400
1923-LFXTAL069404TR-ND LFXTAL069404
1923-LFXTAL078382TR-ND LFXTAL078382
1923-LFXTAL082080TR-ND LFXTAL082080
1923-LFXTAL078207TR-ND LFXTAL078207
1923-LFXTAL082084TR-ND LFXTAL082084
1923-LFXTAL082081TR-ND LFXTAL082081
1923-LFXTAL078719TR-ND LFXTAL078719
1923-LFXTAL082082TR-ND LFXTAL082082
1923-LFXTAL082087TR-ND LFXTAL082087
1923-LFXTAL082088TR-ND LFXTAL082088
1923-LFXTAL082084REELTR-ND LFXTAL082084REEL
1923-LFXTAL082080REELTR-ND LFXTAL082080REEL
1923-LFXTAL082082REELTR-ND LFXTAL082082REEL
1923-LFXTAL082088REELTR-ND LFXTAL082088REEL
1923-LFXTAL078207REELTR-ND LFXTAL078207REEL
1923-LFXTAL078719REELTR-ND LFXTAL078719REEL
1923-LFXTAL082081REELTR-ND LFXTAL082081REEL
1923-LFXTAL071952TR-ND,1923-LFXTAL071952CT-ND LFXTAL071952
1923-LFXTAL072844TR-ND,1923-LFXTAL072844CT-ND,1923-LFXTAL072844DKR-ND LFXTAL072844
1923-LFXTAL081865TR-ND,1923-LFXTAL081865CT-ND LFXTAL081865